Custom compiled U-BOOT fail to boot from eMMC with ext4: ** Unrecognized filesystem type **
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-21 5:08 AM
I have custom complied U-BOOT according this wiki page:
It was build succesfully to support QSPI flash. Now I want to unify it with eMCC, so wand to use same custom compiled TF-A, U-BOOT for both QSPI and eMMC.
After TF-A and U-BOOT (with FIP) build I have successfully downloaded all of them to target board using standard FlashLayout file but after trying to boot eMMC found following message in console:
Hit any key to stop autoboot: 0
Boot over mmc0!
switch to partitions #0, OK
mmc0(part 0) is current device
** Unrecognized filesystem type **
Accoring to mmc part it has correct PT:
STM32MP> mmc part
Partition Map for MMC device 0 -- Partition Type: EFI
Part Start LBA End LBA Name
Attributes
Type GUID
Partition GUID
1 0x00000400 0x000023ff "fip"
attrs: 0x0000000000000000
type: 8da63339-0007-60c0-c436-083ac8230908
guid: 2b0cfe67-d6dd-4c69-a5f4-6aa612222be5
2 0x00002400 0x000223ff "boot"
attrs: 0x0000000000000004
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
type: linux
guid: 2fca1102-25c7-4251-be14-fa2f44bac9c3
3 0x00022400 0x0002a3ff "vendorfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
type: linux
guid: c66dbb14-a7b9-4159-a5be-e8a6d390a494
4 0x0002a400 0x0019f3ff "rootfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
type: linux
guid: e91c4e10-16e6-4c0e-bd0e-77becf4a3582
5 0x0019f400 0x0072bbff "userfs"
attrs: 0x0000000000000000
type: 0fc63daf-8483-4772-8e79-3d69d8477de4
type: linux
guid: 3310aa04-c53f-4693-aa00-08cf60cbb12d
STM32MP>
I've spent some time and discovered, that ext4 fs is disabled by default and can be enabled with CONFIG_FS_EXT4=1 in command line. I use this command to comile:
make -f ../Makefile.sdk DEVICE_TREE=stm32mp157a-stm32mp151-dk1-mx DEPLOYDIR=$FIP_DEPLOYDIR_ROOT/u-boot FIP_CONFIG="trusted" CONFIG_FS_EXT4=1 FIP_BL32_CONF="tfa," all
But there is error diring compile time:
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x50): undefined reference to `ext4fs_probe'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x54): undefined reference to `ext4fs_ls'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x58): undefined reference to `ext4fs_exists'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x5c): undefined reference to `ext4fs_size'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x60): undefined reference to `ext4_read_file'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x64): undefined reference to `ext4_write_file'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x68): undefined reference to `ext4fs_close'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x6c): undefined reference to `ext4fs_uuid'
arm-ostl-linux-gnueabi-ld.bfd: fs/built-in.o:(.data.fstypes+0x84): undefined reference to `ext4fs_create_link'
Could you please give me a way how to enable ext4 support in custome U-BOOT?
I also noticed following things:
- We need to issue command make stm32mp15_trusted_defconfig
.config file will be created in u-boot src root
But after issuing make command above there is strange mastake that U-BOOT src root is not clean and reccommendating to run make mrproper that will remove .config created with make stm32mp15_trusted_defconfig:
Using /home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-2020.10.r1-r0/u-boot-stm32mp-2020.10.r1 as source for U-Boot
/home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-2020.10.r1-r0/u-boot-stm32mp-2020.10.r1 is not clean, please run 'make mrproper'
in the '/home/screep/Distribution-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-03-31/sources/arm-ostl-linux-gnueabi/u-boot-stm32mp-2020.10.r1-r0/u-boot-stm32mp-2020.10.r1' directory.
If I remove CONFIG_FS_EXT4=1 option and rum make mrproper u-boot builds succesfully.
Could you please give a hint to me how to correctly enable ext4 fs in custom u-boot?
Thank you in advance
Looking forward for your reply
- than
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-21 11:25 AM
Finally found right solution here:
https://community.st.com/s/question/0D53W00000HzFR0/i-found-the-env-problem-when-emmc-started
Temporary added env partition to FlashLayout with default evn addredd defined in uboot config.
Here is explanation abount uboot env:
https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_environment_variables
It stored in the end of ssbl partition. How do deal with FIP based images? Should I rename 'ssbl' to 'fip' here:
u-boot,mmc-env-partition = "ssbl";
Anyway currently problem is fully solved and I've god board booted again :)
Thank you in advance
Looking forward for your reply
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-21 6:47 AM
There is update, seems u-boot's etx4 is ok, I can read content of some partitions:
STM32MP> ext4ls mmc 0:0 /
** Unrecognized filesystem type **
STM32MP> ext4ls mmc 0:1 /
** Unrecognized filesystem type **
STM32MP> ext4ls mmc 0:2 /
** Unrecognized filesystem type **
STM32MP> ext4ls mmc 0:3 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
<DIR> 1024 etc
<DIR> 1024 usr
<DIR> 1024 var
STM32MP> ext4ls mmc 0:4 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
<DIR> 2048 bin
<DIR> 1024 boot
<DIR> 1024 dev
<DIR> 1024 etc
<DIR> 1024 home
<DIR> 2048 lib
<DIR> 1024 media
<DIR> 1024 mnt
<DIR> 1024 proc
<DIR> 1024 run
<DIR> 2048 sbin
<DIR> 1024 sys
<DIR> 1024 tmp
<DIR> 1024 usr
<DIR> 1024 var
STM32MP> ext4ls mmc 0:5 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
<DIR> 1024 Cube-M4-examples
<DIR> 1024 Linux-A7-examples
<DIR> 1024 demo
<DIR> 1024 weston-start-at-startup
STM32MP> ext4ls mmc 0:6 /
** Invalid partition 6 **
STM32MP>
May be boot partition set wrong. But board still can't be booted...
Still need help :)
Thank you in advance
Looking forward for your reply
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-21 8:16 AM
And more information. After target programming with CubeMXProgrammer, but before reboot bootfs partition is ok:
STM32MP> ext4ls mmc 0:0 /
** Unrecognized filesystem type **
STM32MP> ext4ls mmc 0:1 /
** Unrecognized filesystem type **
STM32MP> ext4ls mmc 0:2 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
3639 boot.scr.uimg
<DIR> 1024 mmc0_extlinux
<DIR> 1024 mmc1_extlinux
<DIR> 1024 nand0_extlinux
54866 stm32mp157a-stm32mp151-dk1-mx.dtb
7457152 uImage
STM32MP>
After first reboot it look damaged:
STM32MP> ext4ls mmc 0:2 /
** Unrecognized filesystem type **
STM32MP>
Here is log after first reboot:
NOTICE: SP_MIN: v2.4-r1.0(debug):
NOTICE: SP_MIN: Built : 07:47:48, Sep 21 2021
INFO: ARM GICv2 driver initialized
INFO: Set calibration timer to 60 sec
INFO: ETZPC: UART1 (3) could be non secure
INFO: ETZPC: SPI6 (4) could be non secure
INFO: ETZPC: CRYP1 (9) could be non secure
INFO: ETZPC: I2C6 (12) could be non secure
INFO: SP_MIN: Initializing runtime services
INFO: SP_MIN: Preparing exit to normal world
U-Boot 2020.10-stm32mp-r1 (Sep 21 2021 - 12:00:11 +0300)
CPU: STM32MP157DAB Rev.Z
Model: STMicroelectronics STM32MP157A-DK1 STM32CubeMX board
Board: stm32mp1 in trusted mode (st,stm32mp157a-stm32mp151-dk1-mx)
DRAM: 512 MiB
Clocks:
- MPU : 800 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 0
Loading Environment from MMC... *** Warning - bad CRC, using default environment
In: serial
Out: serial
Err: serial
invalid MAC address in OTP 00:00:00:00:00:00
stm32 vrefbuf timed out: -110
adc@0: can't enable vdd-supply!adc_measurement: single shot failed for adc@0[18]!
Net:
Error: ethernet@5800a000 address not set.
No ethernet found.
Hit any key to stop autoboot: 0
Boot over mmc0!
Saving Environment to MMC... Writing to redundant MMC(0)... OK
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:2...
Found U-Boot script /boot.scr.uimg
3639 bytes read in 19 ms (186.5 KiB/s)
## Executing script at c4100000
Executing SCRIPT on target=mmc0
Saving Environment to MMC... Writing to MMC(0)... OK
switch to partitions #0, OK
mmc0(part 0) is current device
** Unrecognized filesystem type **
SCRIPT FAILED... /mmc0_extlinux/extlinux.conf not found !
Saving Environment to MMC... Writing to redundant MMC(0)... OK
SCRIPT FAILED: continuing...
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
STM32MP> STM32MP> ext4ls mmc 0:0 /
Unknown command 'STM32MP>' - try 'help'
STM32MP> ** Unrecognized fSTM32MP> ext4ls mmc 0:1 /
Unknown command '**' - try 'help'
STM32MP> ** Unrecognized filesystem type *DIR> 1024 .
Unknown command '**' - try 'help'
STM32MP> <DIR> 1024 ..
Unknown command '<DIR>' - try 'help'
STM32MP> <DIR> 12288 lost+found
Unknown command '<DIR>' - try 'help'
STM32MP> <DIR> 1024 mmc0_extlinux
Unknown command '<DIR>' - try 'help'
STM32MP> <DIR> 1024 nand0_extlinux
Unknown command '<DIR>' - try 'help'
STM32MP> 54866 s
Unknown command '54866' - try 'help'
STM32MP> 7457152 uImage
Unknown command '7457152' - try 'help'
STM32MP> STM32MP>
Unknown command 'STM32MP>' - try 'help'
STM32MP> ext4ls mmc 0:2 /
** Unrecognized filesystem type **
STM32MP> ext4ls mmc 0:2 /
** Unrecognized filesystem type **
STM32MP> ext4ls mmc 0:3 /
<DIR> 1024 .
<DIR> 1024 ..
<DIR> 12288 lost+found
<DIR> 1024 etc
<DIR> 1024 usr
<DIR> 1024 var
STM32MP> ext4ls mmc 0:2 /
** Unrecognized filesystem type **
STM32MP>
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-21 11:25 AM
Finally found right solution here:
https://community.st.com/s/question/0D53W00000HzFR0/i-found-the-env-problem-when-emmc-started
Temporary added env partition to FlashLayout with default evn addredd defined in uboot config.
Here is explanation abount uboot env:
https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_environment_variables
It stored in the end of ssbl partition. How do deal with FIP based images? Should I rename 'ssbl' to 'fip' here:
u-boot,mmc-env-partition = "ssbl";
Anyway currently problem is fully solved and I've god board booted again :)
Thank you in advance
Looking forward for your reply
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-21 11:49 PM
Hi @ASkri.1​ ,
I confirm an small error in https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_environment_variables
From DV3.0 delivery and default configuration with FIP you should have :
u-boot,mmc-env-partition = "fip";
Olivier
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.