cancel
Showing results for 
Search instead for 
Did you mean: 

Could not load multimedia backend "ffmpeg"

loupi
Associate II

Hello everybody,

i use "meta-st-x-linux-qt"  with "meta-qt6" on STM32MP157

https://github.com/STMicroelectronics/meta-st-x-linux-qt

when I use "QMediaPlayer" to play an audio file it gives me the following error:

 

could not load multimedia backend "ffmpeg" QtMultimedia is not currently supported on this platform or compiler. Aborted (core dumped)

 

if I understand correctly, "ffmpeg" would be missing on my platform, how can I add it to yocto when generating it?

Thank you very much

Loupi

1 REPLY 1
PPAGE.13
ST Employee

Hi,

have you used the "v2.0.0" branch of X-LINUX-QT meta layer?

Normally Qt6 Multimedia should be compiled as well, you can check if libQt6Multimedia.so is in usr/lib.

BR,

Philippe.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.