2020-03-23 12:36 PM
We are using developBoard by Emcraft with STM32MP157A.
Emcraft release board with Openstlinux 4.14.
If I want change devicetree of STM32MP1 i need use STM32CubeMX to export new devicetree.
If i go in STM32CubeMX-->Project Manager-> Project OpenSTLinux setting, I CAN’T CHANGE version of STLinux.
Is it possible to change this setting?
Thanks
Solved! Go to Solution.
2023-10-13 4:55 AM
Hi @AApol.3 , @casparfriedrich ,
You have to use the version of CubeMX corresponding to your ecosystem.
Please refer to release note in wiki . eg for Kernel 5.15 it's ecosystem V4.1 STM32 MPU ecosystem release note - stm32mpu-ecosystem-v4
STM32CubeMX-v6.7.0 might be used.
openstlinux-20-02-19 correspond to ecosystem V1.0 ( deprecated and not recommanded !!) and require CubeMX5.6 for compatible manifests
Olivier
2020-03-25 7:29 AM
Hi @AApol.3
Kernel 4.14 is not supported by ST ecosystem but only by Emcraft.
I invite you to contact Emcraft for further support about tools and ecosystem addressing their SOM product.
BR,
Olivier
2020-03-27 8:52 AM
Hi Oliver,
Thanks for your answer.
we are contatting Emcraft, but if we want use STM32cubeMX to change devicestree of openstlinux-20-02-19, we can not change manifest or Linux version? If we want use old manifest or old Linux version, how we can change theese settings?
Best regards
2023-10-13 4:16 AM - edited 2023-10-13 4:24 AM
Hi,
I have exactly the same problem. I want to use the LTS-Version 5.15 but the "Manifest Version" says "openstlinux-6.1-yocto-mickledore-mp1-v23.06.21". My STM32CubeMX version is 6.9.2 on Linux/Windows and all software packages regarding STM32MP1 are installed.
Best regards
Caspar
2023-10-13 4:55 AM
Hi @AApol.3 , @casparfriedrich ,
You have to use the version of CubeMX corresponding to your ecosystem.
Please refer to release note in wiki . eg for Kernel 5.15 it's ecosystem V4.1 STM32 MPU ecosystem release note - stm32mpu-ecosystem-v4
STM32CubeMX-v6.7.0 might be used.
openstlinux-20-02-19 correspond to ecosystem V1.0 ( deprecated and not recommanded !!) and require CubeMX5.6 for compatible manifests
Olivier
2023-10-23 8:30 AM
Okay, I do get that right, that the solution is to roll back CubeMX? I'll try that later, thanks.