2022-01-31 07:25 AM
Hello, I want to use DDR test suite in STM32 cube IDE but I always have a error when I try to connect my board. I think I understood that was because I have to modify something with stage boot with SPL. I red the docs but I am quite lost can someone give me the steps to make DDR test suite work ?
Kind regards
2022-01-31 07:38 AM
Hi @--.2 ,
Yes indeed DDR Tuning tool require to build and load U-Boot SPL
Please read here :
U-Boot SPL: DDR interactive mode - stm32mpu
Hope it help
Olivier