cancel
Showing results for 
Search instead for 
Did you mean: 

Can we load and run inference an AI model from Cortex M33 of STM32MP257-DK?

Santosh-Italiya
Visitor

Hello,

I am trying to create a project from STMcubeIDE (v1.16.1) for STM32MP257-DK and would like to load a .tflite model on Cortex M33 and run inference to the model. However, when I was creating the project, I brows to my test model from the .ioc file and when I tried to Analyze, It throws the "stm32mp2 component is not available, please install" error. I double checked that the stm32mp2 is already installed. Can anyone please let me know if I am missing anything here. Below are the images for error logs and stm32mp2 installed image.

Error image:

Screenshot 2025-03-10 141851.png

stm32mp2 installed image:

Screenshot 2025-03-10 142223.png

Thank you.

 

0 REPLIES 0