2020-09-22 07:48 AM
2020-09-22 08:15 AM
Hi @FDuch.1 ,
Maybe you can try to add the following layer to your build : https://github.com/OSSystems/meta-browser.
BR,
Christophe
2021-06-22 01:03 PM
I have such an image built using the above named repo. I also had to add meta-clang (make sure to use the dunfell branch) and meta-python2.
T problem is the STMicro Yocto images use Wayland and not X-11. I can't get chromium to start, even though it is also built for Wayland. I keep getting a "cannot open display" error.
Also, be aware it will take over 3 hours for a clean build on a Core i9 with Samsung 980-PRO NVMe so make sure to enable/configure SSTATE and Download caches to reduce subsequent clean build times.
2021-06-25 01:14 PM
While I was able to build the image and get Chromium to somewhat start, it just hung and crashed after a few minutes with nothing displayed.