2022-07-21 7:25 PM
Hi ~
I've designed custom board of STM32MP157C.
1. I created my own device tree using CubeMX refer to the below article.
https://wiki.st.com/stm32mpu/wiki/How_to_create_your_board_device_tree
2. I also created own machine refer to the below article.
https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_machine
3. st-image-weston build was successful.
4. so now, I want to modify the linux kernel device tree.
and I finded article below ..
https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Distribution_Package
Run "devtool modify virtual/kernel" command.
workspace directory was created successfully.
but I can not find my device tree in path below.
./workspace/sources/linux-stm32mp/arch/arm/boot/dts
My device tree files placed at "layers/meta-st/meta-st-stm32mp-addons/mx".
How to solve it ?
Thanks.
Solved! Go to Solution.
2022-07-22 12:09 AM
Hello @hochul yoo,
Your device trees are generated with your Cube MX project. When your project is finished and when you want to use it with your Distribution Package, you have to precize its location in your Yocto machine:
--------------------------
Example:
# CubeMX Project Config
# =========================================================================
# Assign CubeMX Board devicetree and project path name
CUBEMX_DTB = "stm32mp157f-project-mx"
CUBEMX_PROJECT = "MX/STM32MP157F-DK2/<name_project>/CA7/DeviceTree/<name_project>"
# Indicate which STM32MP package are used: 'A', 'C', 'D' or 'F'
CUBEMX_SOC_PACKAGE = "F"
# Indicate the size of DDR available on BOARD: 512 or 1024 (size in MB unit)
CUBEMX_BOARD_DDR_SIZE = "512"
# Indicate if you like to disable the DVFS which are activated by default
#CUBEMX_SOC_DVFS_OFF = "0"
---------------------------------------------
If you want to modify your kernel device tree, you just have to take the one that you have in the MX project linked with your Distribution Package.
Regards.
Erwan.
2022-07-22 12:09 AM
Hello @hochul yoo,
Your device trees are generated with your Cube MX project. When your project is finished and when you want to use it with your Distribution Package, you have to precize its location in your Yocto machine:
--------------------------
Example:
# CubeMX Project Config
# =========================================================================
# Assign CubeMX Board devicetree and project path name
CUBEMX_DTB = "stm32mp157f-project-mx"
CUBEMX_PROJECT = "MX/STM32MP157F-DK2/<name_project>/CA7/DeviceTree/<name_project>"
# Indicate which STM32MP package are used: 'A', 'C', 'D' or 'F'
CUBEMX_SOC_PACKAGE = "F"
# Indicate the size of DDR available on BOARD: 512 or 1024 (size in MB unit)
CUBEMX_BOARD_DDR_SIZE = "512"
# Indicate if you like to disable the DVFS which are activated by default
#CUBEMX_SOC_DVFS_OFF = "0"
---------------------------------------------
If you want to modify your kernel device tree, you just have to take the one that you have in the MX project linked with your Distribution Package.
Regards.
Erwan.