cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157D-DK1 - Recommended DSI Displays

alw
Senior

Hello,

Is there a list of supported/recommended displays that are compatible with the DSI connector CN4 on STM32MP157D-DK1 please?

Kind regards,

Al

 

 

1 REPLY 1
PatrickF
ST Employee

Hi @alw 

few are listed in wiki:

Orise Tech OTM8009a <-- this one is sell into STM32MP157F-DK2 kit

Raspberry Pi 7" Touch

 

Many other might be supported if you are going to build your own board with specific connector.
e.g. this one is provided with STM32MP157F-EV1 kit: Raydium RM68200 

 

Maybe some people in the community are willing to share their information on their used DSI display with STM32MP15x.

 

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here