STM32MP157-DK2 not connecting to ethernet
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-05 9:10 AM
Hello,
i have a problem when tring to establish a ethernet connection with the STM32MP157-DK2 board.
Windows 10 -64bit system, no firewall, no antivirus. DHCP enabled.
Tried with cross & straight CAT6 ethernet cable.
I cannot establish a SSH connection with the board trough putty on port 22.
The yellow LED from the ethernet connector is blinking, the GREN led is off.
In the board "netdata perf monitor" i have no ethernet connection.
I wonder what i am missing here?
Here is the ifconfig
root@stm32mp1:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:80:E1:42:55:EF
inet6 addr: fe80::280:e1ff:fe42:55ef/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:66 errors:0 dropped:0 overruns:0 frame:0
TX packets:48 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:9472 (9.2 KiB) TX bytes:8923 (8.7 KiB)
Interrupt:60 Base address:0x8000
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:264 errors:0 dropped:0 overruns:0 frame:0
TX packets:264 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:16800 (16.4 KiB) TX bytes:16800 (16.4 KiB)
usb0 Link encap:Ethernet HWaddr EE:66:75:77:9F:02
inet addr:192.168.7.2 Bcast:192.168.7.255 Mask:255.255.255.0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@stm32mp1:~#
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-07 4:08 AM
It seems to work, only when i have the cable plugged into the router.
Tried before to connect the board to 2 laptops without success...
How to configure eth0 to run ipv4 with dhcp enabled?
noticed /etc/network/interface file is missing
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-08 7:45 AM
Hello,
Did you visit the ST wiki page: https://wiki.st.com/stm32mpu/wiki/How_to_configure_ethernet_interface ?
It shows you how to configure eth0 /ipv4 with DHCP enabled.
BR
O.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-09 12:53 PM
Hello
i manually configured a ip, on the pc side dhcp is enabled.
After doing this, i still can't connect via ssh, not even ping ..,
Is it posible to disable ipv6? And how to doit?
root@stm32mp1:~# ifconfig eth0 192.168.100.97
root@stm32mp1:~# ifconfig
eth0 Link encap:Ethernet HWaddr 00:80:E1:42:55:EF
inet addr:192.168.100.97 Bcast:192.168.100.255 Mask:255.255.255.0
inet6 addr: fe80::280:e1ff:fe42:55ef/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:99 errors:0 dropped:0 overruns:0 frame:0
TX packets:54 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:11100 (10.8 KiB) TX bytes:10386 (10.1 KiB)
Interrupt:60 Base address:0x8000
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:264 errors:0 dropped:0 overruns:0 frame:0
TX packets:264 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:16800 (16.4 KiB) TX bytes:16800 (16.4 KiB)
usb0 Link encap:Ethernet HWaddr D6:62:9A:22:E4:74
inet addr:192.168.7.2 Bcast:192.168.7.255 Mask:255.255.255.0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@stm32mp1:~# route
Kernel IP routing table
Destination Gateway Genmask Flags Metric Ref Use Iface
192.168.7.0 * 255.255.255.0 U 0 0 0 usb0
192.168.100.0 * 255.255.255.0 U 0 0 0 eth0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-10 2:04 AM
Hi,
you said that via a Router all is correct with DHCP enabled, which is the correct behaviour. Did you try to disable DHCP using a p2p connexion?
I would recommend USB/Ethernet bridge for a P2P connexion. Just plug a USB TypeC cable to the OTG USB DK2 board and type ifconfig again, then manually assign this bridge to a static IP address :ifconfig <bridgename> 192.168.7.1 netmask 255.255.255.0 . Then you should be able to ping the board at 192.168.7.2,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-13 2:49 AM
Hello Oliver,
i tried the followings
- dhcp enabled on the PC side
- power up the DK2 board
- ethernet & usb otg cable connected
- ifconfig eth0 192.168.7.22 netmask 255.255.255.0
- on the pc when ping 192.168.7.22 i get time out response
tried the same with the usb otg connection, and get ping timeout
To be honest its my first approach with a linux embedded system, didn't thought to be such challenging to do a network connection.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-15 2:35 AM
Hello Anton,
Make sure the DK2 board boot pins are set so that you could see a demo on target display screen.
With the Ethernet/USB bridge (using USB type C cable), you should have the following network setup (or similar) from the host side and board side. I've highlighted the bridge which appears when you plug the USB Type C cable. I run linux on a Linux VM on Windows 10.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-15 10:25 AM
Hello Oliver,
thanks for your patience,
i finally managed to establish a ssh connection between my pc and the dk2 board trough USB-C connection.
I setup 192.168.7.1 static ip for my usb network connection on the PC side.
Then i was able to ping 192.168.7.2 board, also ssh worked via putty.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-15 10:26 AM