2022-02-02 7:09 AM
make ARCH=arm uImage vmlinux dtbs LOADADDR=0xC2000040
GEN Makefile
HOSTCC scripts/mod/mk_elfconfig
/media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/usr/bin/ld: /usr/lib/gcc/x86_64-linux-gnu/11/liblto_plugin.so: error loading plugin: /media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/SDK/sysroots/x86_64-ostl_sdk-linux/lib/libc.so.6: version `GLIBC_2.33' not found (required by /usr/lib/gcc/x86_64-linux-gnu/11/liblto_plugin.so)
collect2: error: ld returned 1 exit status
make[2]: *** [scripts/Makefile.host:95: scripts/mod/mk_elfconfig] Error 1
make[1]: *** [/media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.61-stm32mp-r2-r0/linux-5.10.61/Makefile:1214: prepare0] Error 2
make: *** [/media/user/H3D1P2/Tools/STM32MP1/STM_ECO_3.10/Developer-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/sources/arm-ostl-linux-gnueabi/linux-stm32mp-5.10.61-stm32mp-r2-r0/linux-5.10.61/Makefile:185: __sub-make] Error 2
sudo apt-get install libc6
Reading package lists... Done
Building dependency tree... Done
Reading state information... Done
libc6 is already the newest version (2.34-0ubuntu3).
0 upgraded, 0 newly installed, 0 to remove and 0 not upgrad
Linux H3U1 5.13.0-28-lowlatency #31-Ubuntu SMP PREEMPT Thu Jan 13 18:29:33 UTC 2022 x86_64 x86_64 x86_64 GNU/Linux
Solved! Go to Solution.
2022-02-02 7:41 AM
Hello @debugging ,
At this time, we only support up to Ubuntu 20.04 as explained on the wiki: https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Recommended_PC_configurations
Here, if you have done all the steps, the error seems related to the content that you put in bold.
version `GLIBC_2.33' not found (required by /usr/lib/gcc/x86_64-linux-gnu/11/liblto_plugin.so)Our Developer Package is made to use glibc v2.33 and by looking at your traces, the v2.34 is installed on your machine.
Can you try to install glibc v2.33 on your machine and make a symbolic link on this version, to use it by default instead of 2.34.
Otherwise, I recommend you if possible to go back to Ubuntu 20.04, because on 21.10, you will surely encounter other problems.
Regards,
Kevin
2022-02-02 7:18 AM
Hello @debugging ,
Be sure to have made the source of the SDK environment script before trying to build:
PC $> cd $HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Developer-Package
PC $> source SDK/environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabiAnd before building you have to prepare the linux sources as specified in the getting started, in the part 1.1.1.2.3.3 Prepare the Linux® kernel source code of:
This tutorial had been test with Ubuntu 20.04, please tell me if you still have some errors after my recommendation.
Regards,
Kevin
2022-02-02 7:31 AM
Yes , those steps were done and the result shows the error when building the kernel
echo $ARCH
arm
$ echo $CROSS_COMPILE
arm-ostl-linux-gnueabi-
$CC --version
arm-ostl-linux-gnueabi-gcc (GCC) 9.3.0
Copyright (C) 2019 Free Software Foundation, Inc.
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
echo $OECORE_SDK_VERSION
3.1.11-openstlinux-5.10-dunfell-mp1-21-11-17
2022-02-02 7:41 AM
Hello @debugging ,
At this time, we only support up to Ubuntu 20.04 as explained on the wiki: https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Recommended_PC_configurations
Here, if you have done all the steps, the error seems related to the content that you put in bold.
version `GLIBC_2.33' not found (required by /usr/lib/gcc/x86_64-linux-gnu/11/liblto_plugin.so)Our Developer Package is made to use glibc v2.33 and by looking at your traces, the v2.34 is installed on your machine.
Can you try to install glibc v2.33 on your machine and make a symbolic link on this version, to use it by default instead of 2.34.
Otherwise, I recommend you if possible to go back to Ubuntu 20.04, because on 21.10, you will surely encounter other problems.
Regards,
Kevin
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.