Questions about setting the spi clock (devicetree file, M4 Core side)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-21 11:02 PM
Hi ST.
I set the clock in the dts file as below.
&rcc {
st,hsi-cal;
st,csi-cal;
st,cal-sec = <60>;
st,clksrc = <
CLK_MPU_PLL1P
CLK_AXI_PLL2P
CLK_MCU_PLL3P
CLK_PLL12_HSE
CLK_PLL3_HSE
CLK_PLL4_HSE
CLK_RTC_LSE
CLK_MCO1_DISABLED
CLK_MCO2_DISABLED
>;
st,clkdiv = <
1 /*MPU*/
0 /*AXI*/
0 /*MCU*/
1 /*APB1*/
1 /*APB2*/
1 /*APB3*/
1 /*APB4*/
2 /*APB5*/
23 /*RTC*/
0 /*MCO1*/
0 /*MCO2*/
>;
st,pkcs = <
CLK_CKPER_HSI
CLK_QSPI_ACLK
CLK_ETH_DISABLED
CLK_SDMMC12_PLL4P
CLK_STGEN_HSE
CLK_USBPHY_HSE
CLK_SPI2S1_CKPER
CLK_SPI2S23_PLL3Q
CLK_SPI45_PLL4Q
CLK_SPI6_DISABLED
CLK_I2C46_HSI
CLK_SDMMC3_DISABLED
CLK_USBO_USBPHY
CLK_ADC_PLL4R
CLK_CEC_DISABLED
CLK_I2C12_HSI
CLK_I2C35_DISABLED
CLK_UART1_HSI
CLK_UART24_HSI
CLK_UART35_HSI
CLK_UART6_HSI
CLK_UART78_HSI
CLK_SPDIF_DISABLED
CLK_SAI1_DISABLED
CLK_SAI2_DISABLED
CLK_SAI3_DISABLED
CLK_SAI4_DISABLED
CLK_RNG1_LSI
CLK_RNG2_LSI
CLK_LPTIM1_PCLK1
CLK_LPTIM23_PCLK3
CLK_LPTIM45_LSE
>;
/* VCO = 1066.0 MHz => P = 266 (AXI), Q = 533 (GPU), R = 533 (DDR) */
pll2: st,pll@1 {
compatible = "st,stm32mp1-pll";
reg = <1>;
cfg = < 2 65 1 1 0 PQR(1,0,1) >;
frac = <0x1400>;
};
/* VCO = 600.0 MHz => P = 200, Q = 40, R = 60 */
pll3: st,pll@2 {
compatible = "st,stm32mp1-pll";
reg = <2>;
cfg = < 3 99 2 14 9 PQR(1,1,1) >;
/*
frac = <0x1a04>;
*/
};
/* VCO = 792.0 MHz => P = 99, Q = 66, R = 72 */
pll4: st,pll@3 {
compatible = "st,stm32mp1-pll";
reg = <3>;
cfg = < 5 197 7 11 10 PQR(1,1,1) >;
};
};
The following is the SPI setting part of M4 Core Side.
static void MX_SPI5_Init(void)
{
LL_SPI_InitTypeDef SPI_InitStruct = {0};
LL_GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if (IS_ENGINEERING_BOOT_MODE())
{
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SPI45;
PeriphClkInit.Spi45ClockSelection = RCC_SPI45CLKSOURCE_PLL4;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
}
else
{
if (!LL_RCC_PLL4_IsReady())
{
LL_RCC_PLL4_Enable();
}
LL_RCC_PLL4Q_Enable();
}
// Peripheral clock enable
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI5);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOK);
LL_AHB4_GRP1_EnableClock(LL_AHB4_GRP1_PERIPH_GPIOJ);
/* SPI5 GPIO Configuration
PK0 ------> SPI5_SCK
PJ10 ------> SPI5_MOSI
*/
GPIO_InitStruct.Pin = LL_GPIO_PIN_0;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOK, &GPIO_InitStruct);`
GPIO_InitStruct.Pin = LL_GPIO_PIN_10;
GPIO_InitStruct.Mode = LL_GPIO_MODE_ALTERNATE;
GPIO_InitStruct.Speed = LL_GPIO_SPEED_FREQ_MEDIUM;
GPIO_InitStruct.OutputType = LL_GPIO_OUTPUT_PUSHPULL;
GPIO_InitStruct.Pull = LL_GPIO_PULL_NO;
GPIO_InitStruct.Alternate = LL_GPIO_AF_5;
LL_GPIO_Init(GPIOJ, &GPIO_InitStruct);
SPI_InitStruct.TransferDirection = LL_SPI_SIMPLEX_TX;
SPI_InitStruct.Mode = LL_SPI_MODE_MASTER;
SPI_InitStruct.DataWidth = LL_SPI_DATAWIDTH_16BIT;
SPI_InitStruct.ClockPolarity = LL_SPI_POLARITY_LOW;
SPI_InitStruct.ClockPhase = LL_SPI_PHASE_1EDGE;
SPI_InitStruct.NSS = LL_SPI_NSS_SOFT;
SPI_InitStruct.BaudRate = LL_SPI_BAUDRATEPRESCALER_DIV2;
SPI_InitStruct.BitOrder = LL_SPI_MSB_FIRST;
SPI_InitStruct.CRCCalculation = LL_SPI_CRCCALCULATION_DISABLE;
SPI_InitStruct.CRCPoly = 0x0;
LL_SPI_Init(SPI5, &SPI_InitStruct);
LL_SPI_SetStandard(SPI5, LL_SPI_PROTOCOL_MOTOROLA);
}
The following is the part that transmits data using SPI in M4 Core Side.
uint16_t uData = 0xFF0F;
LL_SPI_SetTransferSize(SPI5, 1);
LL_SPI_Enable(SPI5);
LL_SPI_StartMasterTransfer(SPI5);
LL_SPI_TransmitData16(SPI5, uData);
while (LL_SPI_IsActiveFlag_EOT(SPI5) == 0);
LL_SPI_ClearFlag_EOT(SPI5);
LL_SPI_ClearFlag_TXTF(SPI5);
LL_SPI_SuspendMasterTransfer(SPI5);
LL_SPI_Disable(SPI5);
SPI5 uses PLL4Q.
PLL4Q = 66Mhz -> 66/2 -> 33Mhz
The clock of SPI5 should operate at 33Mhz, but as a result of checking with an actual oscilloscope, it is about 2.6Mhz.
When I check it with an oscilloscope in Engineering Mode, it is about 33Mhz, but it is 2.6Mhz in Production Mode (Linux).
Am I wrong clock or SPI5 settings?
Below is the development environment.
Board : Custom board using stm32mp151c chip.
OS : Ecosystem 2.1.0 (202-11-12)
IDE : STM32CubeIDE
Debugger : STLINK-V3SET
Please tell me a solution.
Regards
Machilus
Solved! Go to Solution.
- Labels:
-
STM32MP15 Lines
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-22 5:59 AM
Hello,
Did you use CubeMx ? Is the SPI5 correctly assigned to M4 in the Linux Device Tree ?
You should see something like:
m4_spi5_pins_mx: m4_spi5_mx-0 {
pins {
pinmux = <STM32_PINMUX('J', 10, RSVD)>, /* SPI5_MOSI */
<STM32_PINMUX('J', 11, RSVD)>, /* SPI5_MISO */
<STM32_PINMUX('K', 0, RSVD)>; /* SPI5_SCK */
};
};
.....
&m4_spi5{
pinctrl-names = "default";
pinctrl-0 = <&m4_spi5_pins_mx>;
status = "okay";
};
Otherwise, I think related clock/pll is maybe not setup by Linux (and so SPI5 might be still on pclk2).
Btw, in production mode, GPIO are set by Linux, so using LL_GPIO_Init( ) could result in conflicts hard to debug.
To debug clock, you could also use cat /sys/kernel/debug/clk/clk_summary on Linux to see which frequencies are set in production mode.
Maybe https://wiki.st.com/stm32mpu/wiki/How_to_configure_system_resources#Configuring_clock_and_regulator_system_resources could help you.
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-22 5:59 AM
Hello,
Did you use CubeMx ? Is the SPI5 correctly assigned to M4 in the Linux Device Tree ?
You should see something like:
m4_spi5_pins_mx: m4_spi5_mx-0 {
pins {
pinmux = <STM32_PINMUX('J', 10, RSVD)>, /* SPI5_MOSI */
<STM32_PINMUX('J', 11, RSVD)>, /* SPI5_MISO */
<STM32_PINMUX('K', 0, RSVD)>; /* SPI5_SCK */
};
};
.....
&m4_spi5{
pinctrl-names = "default";
pinctrl-0 = <&m4_spi5_pins_mx>;
status = "okay";
};
Otherwise, I think related clock/pll is maybe not setup by Linux (and so SPI5 might be still on pclk2).
Btw, in production mode, GPIO are set by Linux, so using LL_GPIO_Init( ) could result in conflicts hard to debug.
To debug clock, you could also use cat /sys/kernel/debug/clk/clk_summary on Linux to see which frequencies are set in production mode.
Maybe https://wiki.st.com/stm32mpu/wiki/How_to_configure_system_resources#Configuring_clock_and_regulator_system_resources could help you.
Regards.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-25 1:09 AM
Hi PatrickF (ST Employee)
I modified DTS and Firware by referring to the advice.
I looked at it using the command "cat /sys/kernel/debug/clk/clk_summary" and spi5_k was assigned to "pll4_q".
But didn't solve the problem.
If you set "PCLK2", "HSI", "CSI" and "HSE" in the SPI5 clock mux, it operates normally.
However, only "PLL4Q" does not generate the clock as set.
Is there anything else we need to look into?
P.S : SPI1, SPI2, and SPI3 generate normal clocks as set regardless of the clock source.
Regards
Machilus
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-25 9:54 AM
Hi Machilus (Community Member)
Could you please share your DTS? and .ioc file if generated by CubeMX/CubeIDE?
When you say SPI1, SPI2, and SPI3 generate normal clocks as set, does it includes PLL4_P as clk source for instance?
Regards,
Olivier
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-25 9:10 PM
Hi OlivierK (ST Employee)
Please tell me the e-mail address to send dts and ioc files.
Regards
Machilus
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-01-25 11:40 PM
Hi,
You could send Private Message using pop-up menu which appear when you leave the cursor on a name. You could also uses the Message area.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-04 10:51 AM
Hi Machilus (Community Member)
Regarding the linux side of your configuration, I've found your PLL4 freq out of spec. Did you use CubeMx to modify the clock tree? Also for the M4 configuration it would have been much safer to use this tool to prevent setup errors.
root@stm32mp1:~# cat /sys/kernel/debug/clk/clk_summary
pll4 2 2 0 792000000 0 0 50000
Using your setup, changing the TF-a clock settings on the DK2 board using the spi5 node with the CLK_SPI45_PLLQ
I found spi5_k around 30MHz 0 0 0 29700000 0 0 50000
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-07 4:44 PM
Hi OlivierK (ST Employee)
I entered the same frequency settings into the STM32CubeMX as the shared DTS file, but there are no errors.
If I set "/6" in DIVM4, CubeMX will not throw an error if the condition of "400Mhz =< PLL4 <= 800Mhz" is met.
So setting "792Mhz" in PLL4 didn't cause any warnings or errors in CubeMX.
Is the STM32CubeMX wrong?, We can also share "ioc" files.
I used STM32CubeMX version 6.1.1
I look forward to your reply.
Thanks and regards
Machilus
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-08 6:41 AM
Hi Machilus (Community Member),
For the PLL VCO specifications it is indeed correct, anyway if you've generated your project with CubeMX it should be error free. I did not see the .ioc in the files you've shared, so I was assuming you didn't use CubeMX.
Anyway, I did use you settings in TF-a and regarding the spi5_k do you see the same once booted?
spi5_k 0 0 0 29700000 0 0 50000
Regards,
Olivier
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-08 6:10 PM
Hi OlivierK (ST Employee)
In the picture above, you can see that "spi5_k" is set to 66Mhz in "PLL4Q".
Since the clock setting of "PLL4" is as follows, it is normal that 66Mhz appears in "PLL4Q".
/* VCO = 792.0 MHz => P = 99, Q = 66, R = 72 */
pll4: st,pll@3 {
compatible = "st,stm32mp1-pll";
reg = <3>;
cfg = < 5 197 7 11 10 PQR(1,1,1) >;
};
};
However, if i set the Baudrate of SPI5 of M4 firmware to "LL_SPI_BAUDRATEPRESCALER_DIV2" in production mode booted with Linux, "SPI5_SCK" will output 2.6Mhz instead of 33Mhz.
Regards
Machilus