2020-09-15 8:24 AM
I found that the UBoot env stored at the same address as the bootfs, which caused emMC to fail to start the kernel
Env and Uboot are both at 0x280000 addresses,
Solved! Go to Solution.
2020-09-15 8:49 AM
Hi,
in OpenSTLinux v1.1, for eMMC the enviromnent in saved in ext4 file in bootfs... (CONFIG_ENV_EXT4_FILE = "/uboot.env")
But the U-Boot ext4 suport cause issue as some EXT4 option are not supported in U-Boot to allow write.
in OpenSTLinux v2.0, the eMMC now environment is saved at the END of the U-Boot partition in RAW (CONFIG_ENV_MMC)
https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_environment_variables
And normally CONFIG_ENV_OFFSET is not used for env/mmc.c if "u-boot,mmc-env-partition" is defined in config node of DT
but it can be used as fallback when the partition name is not present in the device tree.
in ST boards, CONFIG_ENV_OFFSET=0X2800000 is used ony for NOR
So I assumed that "u-boot,mmc-env-partition" is missing in your device tree (it is an addition between V1.1 and V2.0)
see ST boards device tree for example
arch/arm/dts/stm32mp157a-dk1-u-boot.dtsi:19:
arch/arm/dts/stm32mp157c-ed1-u-boot.dtsi:20:
/ {
......
config {
.....
u-boot,mmc-env-partition = "ssbl"; <<<<< NEW in v2.0
.....
};
regards
Patrick
2020-09-15 8:49 AM
Hi,
in OpenSTLinux v1.1, for eMMC the enviromnent in saved in ext4 file in bootfs... (CONFIG_ENV_EXT4_FILE = "/uboot.env")
But the U-Boot ext4 suport cause issue as some EXT4 option are not supported in U-Boot to allow write.
in OpenSTLinux v2.0, the eMMC now environment is saved at the END of the U-Boot partition in RAW (CONFIG_ENV_MMC)
https://wiki.st.com/stm32mpu/wiki/U-Boot_overview#U-Boot_environment_variables
And normally CONFIG_ENV_OFFSET is not used for env/mmc.c if "u-boot,mmc-env-partition" is defined in config node of DT
but it can be used as fallback when the partition name is not present in the device tree.
in ST boards, CONFIG_ENV_OFFSET=0X2800000 is used ony for NOR
So I assumed that "u-boot,mmc-env-partition" is missing in your device tree (it is an addition between V1.1 and V2.0)
see ST boards device tree for example
arch/arm/dts/stm32mp157a-dk1-u-boot.dtsi:19:
arch/arm/dts/stm32mp157c-ed1-u-boot.dtsi:20:
/ {
......
config {
.....
u-boot,mmc-env-partition = "ssbl"; <<<<< NEW in v2.0
.....
};
regards
Patrick
2020-12-13 9:34 AM
Hi Patrick,
I trying to change some u-boot variables from user space, and I using u-boot-fw-utils in my Yocto build (2.1 release). I changed the /etc/fw_env.config.mmc to /etc/fw_env.config because I using eMMC ( I did what you mentioned before - u-boot,mmc-env-partition = "ssbl"; )
When I run the program in user space :
root@stm32mp1-ground4-mx:/etc# fw_printenv
Cannot read environment, using default
Cannot read default environment from fileI tried to change the address in /etc/fw_env.config :
/dev/disk/by-partlabel/ssbl -0x2000 0x2000
to address that I think it was with hexdump -C /dev/disk/by-partlabel/ssbl
but nothing changed I still cannot change the env variables.
can you help ?
2020-12-14 5:16 AM
Hi,
Tested on OpenSTLinux v2.1, with alligned U-Boot provided in V2.1 for the ST EV1 board
(v2020.01 => stm32mp15_trusted_defconfig with ENV configuration: CONFIG_ENV_SIZE, CONFIG_ENV_OFFSET_REDUND)
root@stm32mp1:~# fw_printenv -c /etc/fw_env.config.mmc
altbootcmd=run bootcmd
android_mmc_boot=mmc dev ${devnum};run android_mmc_splash;run android_mmc_fdt;run andr;
android_mmc_fdt=if part start mmc ${devnum} dt_${suffix} dt_start &&part size mmc ${dei
android_mmc_kernel=if part start mmc ${devnum} boot_${suffix} boot_start && part size i
android_mmc_splash=if part start mmc ${devnum} splash splash_start && part size mmc ${i
arch=arm
autoload=no
baudrate=115200
board=stm32mp1
board_id=0x1272
board_name=stm32mp157f-dk2
board_rev=0x000c
boot_a_script=load ${devtype} ${devnum}:${distro_bootpart} ${scriptaddr} ${prefix}${sc}
boot_device=mmc
boot_efi_binary=if fdt addr ${fdt_addr_r}; then bootefi bootmgr ${fdt_addr_r};else booi
boot_extlinux=run scan_m4fw;sysboot ${devtype} ${devnum}:${distro_bootpart} any ${scri}
boot_instance=0
boot_m4fw=rproc init; rproc load 0 ${m4fw_addr} ${filesize}; rproc start 0
boot_net_usb_start=true
boot_prefixes=/mmc0_
boot_script_dhcp=boot.scr.uimg
boot_scripts=boot.scr.uimg boot.scr
boot_syslinux_conf=extlinux/stm32mp157f-dk2_extlinux.conf
boot_targets=mmc0
bootcmd=run bootcmd_stm32mp
bootcmd_android=env set mmc_boot run android_mmc_boot;run bootcmd_stm32mp
bootcmd_mmc0=devnum=0; run mmc_boot
bootcmd_mmc1=devnum=1; run mmc_boot
bootcmd_mmc2=devnum=2; run mmc_boot
bootcmd_pxe=run boot_net_usb_start; dhcp; if pxe get; then pxe boot; fi
bootcmd_stm32mp=echo "Boot over ${boot_device}${boot_instance}!";if test ${boot_device;
bootcmd_ubifs0=devnum=0; run ubifs_boot
bootcount=3
bootdelay=1
bootfstype=ext4
cpu=armv7
devplist=4
distro_bootcmd=for target in ${boot_targets}; do run bootcmd_${target}; done
dtimg_addr=0xc44FFF80
efi_dtb_prefixes=/ /dtb/ /dtb/current/
env_check=env exists env_ver || env set env_ver ${ver};if env info -p -d -q; then env ;
env_ver=U-Boot 2020.01-stm32mp-r2.1 (Jan 06 2020 - 20:56:31 +0000)
ethaddr=00:80:e1:42:7c:ce
fastboot.boot_instance=0
fastboot.boot_mode=trusted
fdt_addr_r=0xc4000000
fdtcontroladdr=d7aec640
fdtfile=stm32mp157f-dk2.dtb
fileaddr=c4100000
filesize=b7f
kernel_addr_r=0xc2000000
load_efi_dtb=load ${devtype} ${devnum}:${distro_bootpart} ${fdt_addr_r} ${prefix}${efi}
loadaddr=0xc2000000
m4fw_addr=0xc2000000
m4fw_name=rproc-m4-fw.elf
mmc_boot=if mmc dev ${devnum}; then devtype=mmc; run scan_dev_for_boot_part; fi
partitions=name=ssbl,size=2M;name=bootfs,size=64MB,bootable;name=vendorfs,size=16M;nam-
pxefile_addr_r=0xc4200000
ramdisk_addr_r=0xc4400000
scan_dev_for_boot=echo Scanning ${devtype} ${devnum}:${distro_bootpart}...; for prefix;
scan_dev_for_boot_part=part list ${devtype} ${devnum} -bootable devplist; env exists dt
scan_dev_for_efi=setenv efi_fdtfile ${fdtfile}; if test -z "${fdtfile}" -a -n "${soc}"e
scan_dev_for_extlinux=if test -e ${devtype} ${devnum}:${distro_bootpart} ${prefix}${boi
scan_dev_for_scripts=for script in ${boot_scripts}; do if test -e ${devtype} ${devnum}e
scan_m4fw=if test -e ${devtype} ${devnum}:${distro_bootpart} ${m4fw_name};then echo Fo;
scriptaddr=0xc4100000
serial#=0049002C3438511836383238
serverip=192.168.1.1
soc=stm32mp
splashimage=0xc4300000
suffix=a
ubifs_boot=env exists bootubipart || env set bootubipart UBI; env exists bootubivol ||i
usb_boot=usb start; if usb dev ${devnum}; then devtype=usb; run scan_dev_for_boot_parti
vendor=st
ver=U-Boot 2020.01-stm32mp-r2.1 (Jan 06 2020 - 20:56:31 +0000)
root@stm32mp1:~#
You can add trace in u-boot/env/mmc.c to display the address in eMMC of the expected ENV offset when U-Boot is starting....
Then you can cross check this address used in fw_printenv....
Patrick