cancel
Showing results for 
Search instead for 
Did you mean: 

how to access the adc and dac in stm32mp157d-dk1

Sharan
Senior II

i am using stm32mp157d-dk1 and i am using virtual box and i want to make a gui using c++

which application should i use so that i can access the adc and dac in linux.

using arm cotrex a7 can i access/control the adc and dac. 

for example when I click a button it has to generate sine waves and it has to be written to dac

6 REPLIES 6
GaetanGodart
ST Employee

Hello @Sharan ,

 

Since you seem to start your journey with this MPU serie, I invite you to view this workshop : https://www.youtube.com/watch?v=yD8M_UK4AgQ&list=PLnMKNibPkDnFeV4sBarnsAtFTg7h6V-9_

 

ST made a video for analog DAC on MP1 : https://www.youtube.com/watch?v=NnJ2cTR-eMM

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
PatrickF
ST Employee

Hi @Sharan ,

please have a look to https://wiki.st.com/stm32mpu/wiki/How_to_use_the_IIO_user_space_interface#How_to_do_a_simple_ADC_conversion_using_the_sysfs_interface

ADC is enabled by default OpenSTLinux Device Tree of STM32MP157D-DK1 Starter Package, but not DAC (PA4 and PA5 pins are already used by ADC on the STM32MP157D-DK1).

 

If by ADC and DAC you mean audio codec (available on the board jack), then you should look to https://wiki.st.com/stm32mpu/wiki/ALSA_overview

 

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here
Sharan
Senior II

hii am using stm32mp157d-dk1 and i have downloaded qt creator and i have created a simple hello world window now how to display it in the stm32mp157d-dk1? how to set up cross compilation in order to deploy Qt projects directly from a host Linux machine to the embedded target using qtcreator

Sharan
Senior II

@GaetanGodart @PatrickF 

Regarding distribution package 

after following the bellow steps and  in build-<distro>-<machine>/tmp-glibc/deploy/images/<machine> directory

i cant find the file system image(FlashLayout_sdcard_stm32mp157d-dk1-optee.tsv) in this directory as i am using stm32mp157d-dk1 and it contains for (FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv).can i use FlashLayout_sdcard_stm32mp157f-dk2-optee.tsv itself to flash my stm32mp157d-dk1.

please correct me if the bellow steps are wrong

 

 1.cd <working directory path>/Distribution-Package

2.repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.1-yocto-mickledore-mpu-v24.06.26

3.repo sync

4. DISTRO=openstlinux-weston MACHINE=stm32mp15-disco source layers/meta-st/scripts/envsetup.sh

5.bitbake st-image-weston

6.bitbake st-image-weston -c populate_sdk

7. cd <Distribution Package installation directory>
8.git clone -b v1.0.0 https://github.com/STMicroelectronics/meta-st-x-linux-qt.git layers/meta-st/meta-st-x-linux-qt

9. git clone -b scarthgap https://github.com/meta-qt5/meta-qt5.git layers/meta-qt5

10. source layers/meta-st/scripts/envsetup.sh

11.bitbake-layers add-layer ../layers/meta-qt5 ../layers/meta-st/meta-st-x-linux-qt

12.bitbake st-image-qt

13.bitbake st-image-qt -c populate_sdk

14.bitbake st-image-qt package-index

15.execute "xxx.sh" script available in: build-openstlinuxweston-stm32mp15-disco/tmp-glibc/deploy/sdk

Kevin HUBER
ST Employee

Hello @Sharan ,

If I look at the different machine.conf available, it seems that the board "stm32mp157d-dk1" is only available in the "stm32mp1" machine:

meta-st/meta-st-stm32mp/conf/machine/stm32mp1.conf:56:STM32MP_DT_FILES_SDCARD += "stm32mp157a-dk1 stm32mp157d-dk1"

 

Which is not the case in the "stm32mp15-disco.conf".

So I would say that you have to build your distribution using the MACHINE=stm32mp1

DISTRO=openstlinux-weston MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh


Best Regards,

Kevin

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NEW ! Sidekick STM32 AI agent, see here
Sharan
Senior II

@Kevin HUBER @PatrickF @GaetanGodart how to integrate qt with stm32cubeide for stm32mp157d-dk1 

(beause when a button is clicked in qt it has to write sine values to dac)