2021-03-23 10:34 AM
Hi,
we are currently bring up our custom STM32MP157 Board.
We get in any constellation a
"DDR addr bus test: can't access memory @ 0xc000004"
We think that our crystal is correctly running at 24 Mhz because we connecting over USB to the Board. Also the Voltages is correctly. We use the same DDR Chip, that is on the DK2 ( Micron ), with the same settings.
We run a little bit out of ideas how to handle this. We also got DDR errors in Uboot SPL.
Have you any hints beyond the "Bring up" Guide?
Best regards
Solved! Go to Solution.
2021-04-02 11:12 AM
Hi @Niklas Voi (Community Member)
Have you run DDR tool and applied the DDR tuning values in the DT using #define DDR_PHY_CAL_SKIP, and you have this error at boot on TF-A?
If the answer is yes, then it is a tool limitation that will be corrected in CubeMx v6.3 (limitation is present on CubeMX v6.2).
An issue has been identified regarding DQS Gating (function call missing) and will be corrected in next release of CubeMx/DDR tool (v6.3).
depending if you are in 16-bit DDR or 32-bit DDR, you need to update manually the registers below according to DQS gating values found by DDR tuning.
According to DQS gating values found by DDR tuning.
I hope it'll solve the issue.
Olivier
Here's the workaround.
You still can run DDR tool and apply the calibration values from the test, but you'll need to update, at most, 4 registers manually if you want to include the DQS values in the DT.
https://wiki.st.com/stm32mpu/wiki/DDRCTRL_and_DDRPHYC_device_tree_configuration
In my case (16-bit DDR)
DDR>step 3
current step is 3:DDR_READY
DDR>tuning 0
execute 0:Read DQS gating
Byte 0, R0DGSL = 2, R0DGPS = 0
Byte 1, R0DGSL = 2, R0DGPS = 0
Result: Pass []
-> According to the DQS gating above and the corresponding table (shown below), I need to update manually DX0DQSTR, DX1DQSTR as follow
DX0DQSTR 0x3DB00002
DX1DQSTR 0x3DB00002
For a 32-bit DDR you will have also Byte2, Byte3 showing values.
update manually the 4 registers : DX0DQSTR/DX1DQSTR/DX2DQSTR/DX3DQSTR
Here's the corresponding table to update the registers according to DQS values:
Example for Byte 0 with all combinations from DQS Gating,
( same table for Byte1 = DX1DQSTR, Byte2 = DX2DQSTR, Byte3 =DX3DQSTR)
Byte 0, R0DGSL = 0, R0DGPS = 0 => DX0DQSTR = 0x3DB00000
Byte 0, R0DGSL = 0, R0DGPS = 1 => DX0DQSTR = 0x3DB01000
Byte 0, R0DGSL = 0, R0DGPS = 2 => DX0DQSTR = 0x3DB02000
Byte 0, R0DGSL = 0, R0DGPS = 3 => DX0DQSTR = 0x3DB03000
Byte 0, R0DGSL = 1, R0DGPS = 0 => DX0DQSTR = 0x3DB00001
Byte 0, R0DGSL = 1, R0DGPS = 1 => DX0DQSTR = 0x3DB01001
Byte 0, R0DGSL = 1, R0DGPS = 2 => DX0DQSTR = 0x3DB02001
Byte 0, R0DGSL = 1, R0DGPS = 3 => DX0DQSTR = 0x3DB03001
Byte 0, R0DGSL = 2, R0DGPS = 0 => DX0DQSTR = 0x3DB00002
Byte 0, R0DGSL = 2, R0DGPS = 1 => DX0DQSTR = 0x3DB01002
Byte 0, R0DGSL = 2, R0DGPS = 2 => DX0DQSTR = 0x3DB02002
Byte 0, R0DGSL = 2, R0DGPS = 3 => DX0DQSTR = 0x3DB03002
Byte 0, R0DGSL = 3, R0DGPS = 0 => DX0DQSTR = 0x3DB00003
Byte 0, R0DGSL = 3, R0DGPS = 1 => DX0DQSTR = 0x3DB01003
Byte 0, R0DGSL = 3, R0DGPS = 2 => DX0DQSTR = 0x3DB02003
Byte 0, R0DGSL = 3, R0DGPS = 3 => DX0DQSTR = 0x3DB03003
Byte 0, R0DGSL = 4, R0DGPS = 0 => DX0DQSTR = 0x3DB00004
Byte 0, R0DGSL = 4, R0DGPS = 1 => DX0DQSTR = 0x3DB01004
Byte 0, R0DGSL = 4, R0DGPS = 2 => DX0DQSTR = 0x3DB02004
Byte 0, R0DGSL = 4, R0DGPS = 3 => DX0DQSTR = 0x3DB03004
Byte 0, R0DGSL = 5, R0DGPS = 0 => DX0DQSTR = 0x3DB00005
Byte 0, R0DGSL = 5, R0DGPS = 1 => DX0DQSTR = 0x3DB01005
Byte 0, R0DGSL = 5, R0DGPS = 2 => DX0DQSTR = 0x3DB02005
Byte 0, R0DGSL = 5, R0DGPS = 3 => DX0DQSTR = 0x3DB03005
Byte 0, R0DGSL = 6, R0DGPS = 0 => DX0DQSTR = 0x3DB00006
Byte 0, R0DGSL = 6, R0DGPS = 1 => DX0DQSTR = 0x3DB01006
Byte 0, R0DGSL = 6, R0DGPS = 2 => DX0DQSTR = 0x3DB02006
Byte 0, R0DGSL = 6, R0DGPS = 3 => DX0DQSTR = 0x3DB03006
Byte 0, R0DGSL = 7, R0DGPS = 0 => DX0DQSTR = 0x3DB00007
Byte 0, R0DGSL = 7, R0DGPS = 1 => DX0DQSTR = 0x3DB01007
Byte 0, R0DGSL = 7, R0DGPS = 2 => DX0DQSTR = 0x3DB02007
Byte 0, R0DGSL = 7, R0DGPS = 3 => DX0DQSTR = 0x3DB03007
2021-03-24 9:08 AM
Hi,
did your check the HSE bypass setting in DT ?
did you have an STPMIC1 on your board ?
Is DDR_VREF present at right voltage on STM32MP1 and DDR3L ?
Are DDR_ZQ 240 ohms resistors present on STM32MP1 and DDR3L?
Are DDR_CKE and DDR_RESETN going high ?
Is there clock present on the DDR_CLKP/N ?
Regards.
2021-03-29 7:54 AM
Hi @Niklas Voi
Did you run DDR tuning Tool and apply result settings ?
Olivier
2021-04-02 11:12 AM
Hi @Niklas Voi (Community Member)
Have you run DDR tool and applied the DDR tuning values in the DT using #define DDR_PHY_CAL_SKIP, and you have this error at boot on TF-A?
If the answer is yes, then it is a tool limitation that will be corrected in CubeMx v6.3 (limitation is present on CubeMX v6.2).
An issue has been identified regarding DQS Gating (function call missing) and will be corrected in next release of CubeMx/DDR tool (v6.3).
depending if you are in 16-bit DDR or 32-bit DDR, you need to update manually the registers below according to DQS gating values found by DDR tuning.
According to DQS gating values found by DDR tuning.
I hope it'll solve the issue.
Olivier
Here's the workaround.
You still can run DDR tool and apply the calibration values from the test, but you'll need to update, at most, 4 registers manually if you want to include the DQS values in the DT.
https://wiki.st.com/stm32mpu/wiki/DDRCTRL_and_DDRPHYC_device_tree_configuration
In my case (16-bit DDR)
DDR>step 3
current step is 3:DDR_READY
DDR>tuning 0
execute 0:Read DQS gating
Byte 0, R0DGSL = 2, R0DGPS = 0
Byte 1, R0DGSL = 2, R0DGPS = 0
Result: Pass []
-> According to the DQS gating above and the corresponding table (shown below), I need to update manually DX0DQSTR, DX1DQSTR as follow
DX0DQSTR 0x3DB00002
DX1DQSTR 0x3DB00002
For a 32-bit DDR you will have also Byte2, Byte3 showing values.
update manually the 4 registers : DX0DQSTR/DX1DQSTR/DX2DQSTR/DX3DQSTR
Here's the corresponding table to update the registers according to DQS values:
Example for Byte 0 with all combinations from DQS Gating,
( same table for Byte1 = DX1DQSTR, Byte2 = DX2DQSTR, Byte3 =DX3DQSTR)
Byte 0, R0DGSL = 0, R0DGPS = 0 => DX0DQSTR = 0x3DB00000
Byte 0, R0DGSL = 0, R0DGPS = 1 => DX0DQSTR = 0x3DB01000
Byte 0, R0DGSL = 0, R0DGPS = 2 => DX0DQSTR = 0x3DB02000
Byte 0, R0DGSL = 0, R0DGPS = 3 => DX0DQSTR = 0x3DB03000
Byte 0, R0DGSL = 1, R0DGPS = 0 => DX0DQSTR = 0x3DB00001
Byte 0, R0DGSL = 1, R0DGPS = 1 => DX0DQSTR = 0x3DB01001
Byte 0, R0DGSL = 1, R0DGPS = 2 => DX0DQSTR = 0x3DB02001
Byte 0, R0DGSL = 1, R0DGPS = 3 => DX0DQSTR = 0x3DB03001
Byte 0, R0DGSL = 2, R0DGPS = 0 => DX0DQSTR = 0x3DB00002
Byte 0, R0DGSL = 2, R0DGPS = 1 => DX0DQSTR = 0x3DB01002
Byte 0, R0DGSL = 2, R0DGPS = 2 => DX0DQSTR = 0x3DB02002
Byte 0, R0DGSL = 2, R0DGPS = 3 => DX0DQSTR = 0x3DB03002
Byte 0, R0DGSL = 3, R0DGPS = 0 => DX0DQSTR = 0x3DB00003
Byte 0, R0DGSL = 3, R0DGPS = 1 => DX0DQSTR = 0x3DB01003
Byte 0, R0DGSL = 3, R0DGPS = 2 => DX0DQSTR = 0x3DB02003
Byte 0, R0DGSL = 3, R0DGPS = 3 => DX0DQSTR = 0x3DB03003
Byte 0, R0DGSL = 4, R0DGPS = 0 => DX0DQSTR = 0x3DB00004
Byte 0, R0DGSL = 4, R0DGPS = 1 => DX0DQSTR = 0x3DB01004
Byte 0, R0DGSL = 4, R0DGPS = 2 => DX0DQSTR = 0x3DB02004
Byte 0, R0DGSL = 4, R0DGPS = 3 => DX0DQSTR = 0x3DB03004
Byte 0, R0DGSL = 5, R0DGPS = 0 => DX0DQSTR = 0x3DB00005
Byte 0, R0DGSL = 5, R0DGPS = 1 => DX0DQSTR = 0x3DB01005
Byte 0, R0DGSL = 5, R0DGPS = 2 => DX0DQSTR = 0x3DB02005
Byte 0, R0DGSL = 5, R0DGPS = 3 => DX0DQSTR = 0x3DB03005
Byte 0, R0DGSL = 6, R0DGPS = 0 => DX0DQSTR = 0x3DB00006
Byte 0, R0DGSL = 6, R0DGPS = 1 => DX0DQSTR = 0x3DB01006
Byte 0, R0DGSL = 6, R0DGPS = 2 => DX0DQSTR = 0x3DB02006
Byte 0, R0DGSL = 6, R0DGPS = 3 => DX0DQSTR = 0x3DB03006
Byte 0, R0DGSL = 7, R0DGPS = 0 => DX0DQSTR = 0x3DB00007
Byte 0, R0DGSL = 7, R0DGPS = 1 => DX0DQSTR = 0x3DB01007
Byte 0, R0DGSL = 7, R0DGPS = 2 => DX0DQSTR = 0x3DB02007
Byte 0, R0DGSL = 7, R0DGPS = 3 => DX0DQSTR = 0x3DB03007
2021-04-11 11:34 PM
Hello,
thanks for your help and advice. In the end we got a mix between different errors.
we got a hardware issue on layout. We are now at a point, that the kernel starts and getting the system up.
best regards,
Niklas
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.