cancel
Showing results for 
Search instead for 
Did you mean: 

BOOT From eMMC on SDMMC2 in 4-bit mode

Jboui.450
Associate

Hello,

we would like to boot from a eMMC memory on our board connected to SDMMC2.

As the camera interface is in conflic with SDMMC2 8bit mode, we must configure it as a SDMMC 4 bit width.

The question is will we still me able to boot from our eMMC memory in 4 bit mode as we do in 8 bit ?

The memory we use is the following MTFC4GACAJCN-1M from Micron

Tanks for your support.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PatrickF
ST Employee

At HW level, there is no issue to use 4-bit eMMC as BootROM first boot level only use one data line, e.g. CLK/CMD and D0 on PE3/PG6 and PB14 (see AN5031).

To restrict usage to 4-bit eMMC in TF-A and uBoot/Linux, you should adapt the Device Tree.

Please note that we currently have a limitation for eMMC boot from Micron devices, see ES0438. Meanwhile you should use Toshiba or Kingston devices. This will be solved in future silicon.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Tip of the day: Try Sidekick STM32 AI agent, see here