cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to create debug filesystem

gmax
Visitor

Hello, 

I enabled the generation of  debug filesystem by adding two variables in file build-openstlinuxweston-stm32mp15-disco/conf/local.conf as shown below to use with GDB. This step is  also mentioned in Yocto documentation (Link: https://docs.yoctoproject.org/dev/dev-manual/debugging.html#using-the-gdbserver-method ). 

 

IMAGE_GEN_DEBUGFS = "1"
IMAGE_FSTYPES_DEBUGFS = "tar.bz2"

 

When this option is enabled I get below dependency(?) error,

gmax_3-1721526322507.png

 

Does anyone know how to fix this?


Additional information:

Target HW : STM32MP157F-DK2

Target image : st-image-weston

gmax_2-1721526131690.png

Thanks,

 

 

0 REPLIES 0