2024-02-07 10:05 AM
I need to use the tc358867 bridge in my project. However, the hardware uses the clock that comes from the DSI. The chip's operating cycle requires the clock that comes from the dsi to start working and be found on the i2c bus. I am unable to activate the DSI clock during driver initialization so that I can activate my bridge. Is it possible to use a DSI dummy to inject the clock signal?