cancel
Showing results for 
Search instead for 
Did you mean: 

STM32MP157C-DK2 installing node.js without rebuilding image

Lukas1
Associate III

Hi,

i want to use node.js on STM32MP157C-DK2. I found this post https://community.st.com/s/question/0D50X0000B0xovG/installing-nodejs-on-the-stm32mp1 , but I dont want to rebuild the image

Is there a way to install node.js without rebuilding the image?

I tried this raspberryPi-tutorial: https://www.instructables.com/id/Install-Nodejs-and-Npm-on-Raspberry-Pi/

This works fine until I want to check the version with

node -v

I get following error:

node: error while loading shared libraries: libatomic.so.1: cannot open shared object file: No such file or directory 

thanks in advance

Lukas

1 ACCEPTED SOLUTION

Accepted Solutions
Olivier GALLIEN
ST Employee

Hi @Lukas​ 

OpenSTLinux support apt-get service. See :

https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution

Didn't check but quite sure nodejs package is available.

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Olivier GALLIEN
ST Employee

Hi @Lukas​ 

OpenSTLinux support apt-get service. See :

https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution

Didn't check but quite sure nodejs package is available.

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @Community member​ ,

installing node.js with apt-get worked fine��

If I want to install npm

apt-get install nodejs-npm

I get following error

E: You don't have enough free space in /var/cache/apt/archives/.

But I think there is enough disk-space:

Filesystem      Size  Used Avail Use% Mounted on
/dev/root       715M  682M     0 100% /
devtmpfs        150M     0  150M   0% /dev
tmpfs           214M     0  214M   0% /dev/shm
tmpfs           214M   12M  203M   6% /run
tmpfs           214M     0  214M   0% /sys/fs/cgroup
tmpfs           214M  4.0K  214M   1% /tmp
/dev/mmcblk0p4   58M  8.5M   46M  16% /boot
/dev/mmcblk0p7   14G   74M   13G   1% /usr/local
tmpfs           214M   80K  214M   1% /var/volatile
/dev/mmcblk0p5   15M  8.4M  5.1M  63% /vendor

regards

Lukas