2020-05-20 12:02 AM
Hi,
i want to use node.js on STM32MP157C-DK2. I found this post https://community.st.com/s/question/0D50X0000B0xovG/installing-nodejs-on-the-stm32mp1 , but I dont want to rebuild the image
Is there a way to install node.js without rebuilding the image?
I tried this raspberryPi-tutorial: https://www.instructables.com/id/Install-Nodejs-and-Npm-on-Raspberry-Pi/
This works fine until I want to check the version with
node -v
I get following error:
node: error while loading shared libraries: libatomic.so.1: cannot open shared object file: No such file or directory
thanks in advance
Lukas
Solved! Go to Solution.
2020-05-20 12:13 AM
Hi @Lukas
OpenSTLinux support apt-get service. See :
https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution
Didn't check but quite sure nodejs package is available.
Hope it help
Olivier
2020-05-20 12:13 AM
Hi @Lukas
OpenSTLinux support apt-get service. See :
https://wiki.st.com/stm32mpu/wiki/Package_repository_for_OpenSTLinux_distribution
Didn't check but quite sure nodejs package is available.
Hope it help
Olivier
2020-05-25 1:06 AM
Hi @Community member ,
installing node.js with apt-get worked fine:thumbs_up:
If I want to install npm
apt-get install nodejs-npm
I get following error
E: You don't have enough free space in /var/cache/apt/archives/.
But I think there is enough disk-space:
Filesystem Size Used Avail Use% Mounted on
/dev/root 715M 682M 0 100% /
devtmpfs 150M 0 150M 0% /dev
tmpfs 214M 0 214M 0% /dev/shm
tmpfs 214M 12M 203M 6% /run
tmpfs 214M 0 214M 0% /sys/fs/cgroup
tmpfs 214M 4.0K 214M 1% /tmp
/dev/mmcblk0p4 58M 8.5M 46M 16% /boot
/dev/mmcblk0p7 14G 74M 13G 1% /usr/local
tmpfs 214M 80K 214M 1% /var/volatile
/dev/mmcblk0p5 15M 8.4M 5.1M 63% /vendor
regards
Lukas