Skip to main content
JWali
Associate II
Jul 1, 2019 3:46 AM UTC
Question

Installing Node.js on the STM32MP1

Any recommendations on how to install Node.js on OpenSTLinux / OpenEmbedded?

I want to run some node.js applications on the A7 processor.

I found this repository but there has been no activity for a few years.

https://github.com/imyller/meta-nodejs

This topic has been closed for replies.

13 replies

Olivier GALLIEN
ST Technical Moderator
Jul 1, 2019 8:02 AM UTC

Hi,

Using Yocto layer is the right way to go :

https://wiki.st.com/stm32mpu/wiki/How_to_integrate_an_external_software_package

I can not comment about the package itself, but it looks properly supported byt the community :

https://layers.openembedded.org/layerindex/branch/master/layer/meta-nodejs/

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
JWali
JWaliAuthor
Associate II
Jul 30, 2019 3:17 AM UTC

@Community member​  - Thanks for the tip. I read through https://wiki.st.com/stm32mpu/wiki/How_to_integrate_an_external_software_package and want to install the layer / recipe for Node.js - https://layers.openembedded.org/layerindex/branch/master/layer/meta-nodejs/

I read through https://wiki.st.com/stm32mpu/wiki/OpenSTLinux_distribution and https://wiki.st.com/stm32mpu/wiki/How_to_create_a_new_open_embedded_layer

I also read https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package

Do I really need to cross-compile the entire OpenSTLinux_distribution and create an image to add the node.js layer?

-- John

gokhannsahin
Associate III
Jul 30, 2019 9:41 AM UTC

I too have a error about nodejs while installing meta-iot-cloud.

Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make -j 6 BUILDTYPE=Release
| make -C out BUILDTYPE=Release V=1
| touch ffec8618e06f50f8c62e1ff635021f102d0a41d4.intermediate
| LD_LIBRARY_PATH=/home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/lib.host:/home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/lib.target:$LD_LIBRARY_PATH; export LD_LIBRARY_PATH; cd ../deps/v8/src/inspector; mkdir -p /home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/obj/gen/src/inspector/protocol /home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/obj/gen/include/inspector; python ../../third_party/inspector_protocol/CodeGenerator.py --jinja_dir ../../third_party --output_base "/home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/obj/gen/src/inspector" --config inspector_protocol_config.json
| make[1]: execvp: printf: Argument list too long
| deps/v8/src/v8_base.target.mk:633: recipe for target '/home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/obj.target/deps/v8/src/libv8_base.a' failed
| make[1]: *** [/home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/obj.target/deps/v8/src/libv8_base.a] Error 127
| rm ffec8618e06f50f8c62e1ff635021f102d0a41d4.intermediate
| Makefile:88: recipe for target 'node' failed
| make: *** [node] Error 2
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Function failed: do_compile (log file is located at /home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_eglfs-linux-gnueabi/nodejs/8.12.0-r0/temp/log.do_compile.5426)

gokhannsahin
Associate III
Aug 1, 2019 1:51 PM UTC

I'm still getting this error while compiling nodejs? Should I change the nodejs versions?

JWali
JWaliAuthor
Associate II
Aug 27, 2019 1:40 PM UTC

While cross compiling the meta-iot-cloud layer, it fails to compile nodejs 8.12 with the same error as above:

| make[1]: execvp: printf: Argument list too long
| make[1]: *** [/home/walicki/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out/Release/obj.target/deps/v8/src/libv8_base.a] Error 127
| rm 87e866e2a67de632e2bf83828b5ea47ee79645b4.intermediate
| make[1]: Leaving directory `/home/walicki/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi/nodejs/8.12.0-r0/node-v8.12.0/out'
| make: *** [node] Error 2
| ERROR: oe_runmake failed
| WARNING: /home/walicki/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi/nodejs/8.12.0-r0/temp/run.do_compile.10771:1 exit 1 from 'exit 1'
| ERROR: Function failed: do_compile (log file is located at /home/walicki/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxweston-stm32mp1/tmp-glibc/work/cortexa7t2hf-neon-vfpv4-openstlinux_weston-linux-gnueabi/nodejs/8.12.0-r0/temp/log.do_compile.10771)
ERROR: Task (/home/walicki/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/layers/meta-openembedded/meta-oe/recipes-devtools/nodejs/nodejs_8.12.0.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1903 tasks of which 1591 didn't need to be rerun and 2 failed.
NOTE: Writing buildhistory
 
Summary: 2 tasks failed:
 virtual:native:/home/walicki/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/layers/meta-openembedded/meta-oe/recipes-devtools/nodejs/nodejs_8.12.0.bb:do_compile
 /home/walicki/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/layers/meta-openembedded/meta-oe/recipes-devtools/nodejs/nodejs_8.12.0.bb:do_compile

JWali
JWaliAuthor
Associate II
Aug 27, 2019 1:52 PM UTC

There is a long discussion on this Yocto node / openssl builddir compile issue here:

https://github.com/imyller/meta-nodejs/issues/9

I still don't know the magic incantation.

JWali
JWaliAuthor
Associate II
Aug 28, 2019 3:30 AM UTC

Thanks to a tip from a ST engineer, I have created a file called "nodejs_%.bbappend" with these contents 

   EXTRA_OEMAKE += "builddir_name=."

in this directory:

$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/layers/meta-openembedded/meta-oe/recipes-devtools/nodejs

and added a stanza to

$HOME/STM32MPU_workspace/STM32MP15-Ecosystem-v1.0.0/Starter-Package/stm32mp1-openstlinux-4.19-thud-mp1-19-02-20/layers/meta-openembedded/meta-oe/conf/layer.conf

to include nodejs

IMAGE_INSTALL_append += "nodejs"

I'm finally able to compile and build an image that includes node.js

gokhannsahin
Associate III
Aug 28, 2019 5:06 AM UTC

Thank you @JWali​ 

I get errors while compiling.

ERROR: Nothing RPROVIDES 'nodejsopenssh-sftp' (but /home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/layers/meta-st/meta-st-openstlinux/recipes-samples/images/st-example-image-qt.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target 'nodejsopenssh-sftp' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['nodejsopenssh-sftp']
ERROR: Required build target 'st-example-image-qt' has no buildable providers.
Missing or unbuildable dependency chain was: ['st-example-image-qt', 'nodejsopenssh-sftp']

I have created nodejs_8.12.0.bbappend file and added EXTRA_OEMAKE += "build-openstlinuxeglfs-stm32mp1=." line.

CPRIO
Visitor II
Aug 28, 2019 7:14 AM UTC

Hi,

The append instruction of IMAGE_INSTALL_append dos not add space on your IMAGE_INSTALL variable that means you have concatenated the existing content of IMAGE_INSTALL and 'nodejs' is why you see 'nodejsopenssh-sftp'.

To solve it you need to add space:

IMAGE_INSTALL_append = " nodejs "

christophe

gokhannsahin
Associate III
Aug 28, 2019 9:56 AM UTC

I have generated image with bitbake st-example-image-qt command after added nodejs to local.conf .

However, after added meta-iot-cloud to local.conf with CORE_IMAGE_EXTRA_INSTALL += "packagegroup-cloud-google", it gives the following erros;

ERROR: nodejs-native-8.12.0-r0 do_compile: oe_runmake failed
ERROR: nodejs-native-8.12.0-r0 do_compile: Function failed: do_compile (log file is located at /home/gokhan/STM32MP15-Ecosystem-v1.0.0/Distribution-Package/openstlinux-4.19-thud-mp1-19-02-20/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/x86_64-linux/nodejs-native/8.12.0-r0/temp/log.do_compile.28025)

Olivier GALLIEN
ST Technical Moderator
Jan 14, 2020 9:26 AM UTC

Hi,

Sorry for late reply.

Applying attached patch 0001-nodejs-bump-to-10.16.2 in Distribution package might fix the compilation issue by getting a more recent nodejs version.

  apply patch 0001-nodejs-bump-to-10.16.2.patch on meta-st-openstlinux

   put the following line on conf/local.conf

      PREFERRED_VERSION_nodejs = "10%"

      PREFERRED_VERSION_nodejs-native = "10%"

   and you must have:

      $> bitbake -s | grep node

         nodejs                                            :8.12.0-r0              :10.16.2-r0

         nodejs-native                                     :8.12.0-r0              :10.16.2-r0

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.