cancel
Showing results for 
Search instead for 
Did you mean: 

Expanding SDK and distribution with extra libraries.

CBram.1776
Associate II

Hello, I received the STM32MP1 discovery kit and I started to use it.

I installed SDK and I compiled successfully some hello world applications.

Now, I would like to build some extra libraries to add, or in the future I may want to rebuild existing ones with newer versions.

These packages are typically distributed with a configure script made with autotools, or with CMake build scripts, or with other less widespread tools.

I would like to know what are the options to be used for correct integration with SDK and inside the OpenSTLinux distribution.

For example, with autotools you may need to set options like "--bindir", "--includedir", etc, or CMake needs to receive the right information from an external file assigned to the CMAKE_TOOLCHAIN_FILE macro.

After that, you usually build with "make" and "make install" and you did the job.

What are the recommended options for expanding SDK?

Thank you very much for your time.

Sincerely.

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @CBram.1776​ 

Extension/customization of SDK and Distribution can be made through Yocto.

Guess you can find useful information under wiki user guide https://wiki.st.com/stm32mpu

For example :

https://wiki.st.com/stm32mpu/wiki/How_to_create_an_SDK_for_OpenSTLinux_distribution

https://wiki.st.com/stm32mpu/wiki/How_to_integrate_an_external_software_package

Does it answer your question ?

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.