cancel
Showing results for 
Search instead for 
Did you mean: 

which processor should i used to play high resolution video above 1080P ,

asadullah4571
Associate III

Hi ST Team ,

previously i used the MP1 processor where the video lagging issues, so know i decided to move on another processor who can play the high resolution video above 1080 P @30FPS, 
Note: i do not want any HDMI IC's  , i want direct pin(RGB) through the processor to our HDMI port,

please suggest me which Processor should be better.

9 REPLIES 9
PatrickF
ST Employee

Hi @asadullah4571 

STM32MP2 series are able to play 1080p60 thru LTDC in RGB (depending on blanking required).

Note that ~150MHz clock with 24 bits RGB parallel data bus is challenging in term of general power noise and signal integrity. LTDC bus must be very short and with very low capacitive load.

We recommend to use DSI which could go up to 2048 × 1536 60 fps with much less pins and far much easier signal integrity as using low voltage differential pairs.

 

On STM32MP257F-DK board, we provide 1080p60 HDMI using the onboard DSI2HDMI converter (ADV7535BCBZ).

 

Regards

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @PatrickF 

I am making the project on STM32mp257 board, as you suggested but i want to  know form your side that, will it support for Chromium browser or Firefox?. in your yocto Distribution package there will be no issues with font decoding and as well as video playing.


Hi,

I don't know, MPUs product with embedded Linux are not focusing to be used with 'PC-like' browsers. You could evaluate on your side using STM32MP257F-EV board.

As far as I know, when product has an UI, it is usually done using Weston/Wayland/Gtk or Qt.

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Hi @PatrickF 

I added the 3rd party layers meta-browser with x11 for MP1 board, it works and when i try to play the youtube video, it works but so much lagging issue. So i decided to move on MP2

Now I am going to purchase MP2- DK or EV board, but it should be play youtube video minimum 1080@60 without any lagging issue using  DSI2HDMI  converter . and i will use  2GB RAM DDR4.
please suggest me will it works?

@asadullah4571 @PatrickF 

I want to use MP2 as a simple notebook.

Any progress about youtube on the MP2-dev board?

Looking forward for your reply!

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

@Andrew Neil  yes i know.

I'm just looking for a reply from @asadullah4571 

STM32MP151AAC3 custom board with STM32-OS as operating system: https://github.com/DanielMartensson/STM32-Computer

You know, but others in this thread might not have seen your other threads on the same topic

hi @DMårt

Actually i done this on MP1 processor and works fine, becouse of the same branch "krikstone" will support on MP1 as well as Meta-browser.

and I try to build the krikstone branch with MP2 i got the error. "machine target not found". so simply not possible to add meta-browser layer into the Distro package.