2024-05-13 2:24 AM
I enabled fmc in arch/arm/boot/dts/stm32mp157f-dk2.dts:
&fmc {
status = "okay";
};
And this is how i read or write its registers:
static inline unsigned int readl(const volatile void *addr)
{
unsigned int val;
__asm__ __volatile__("": : :"memory");
val = *(volatile unsigned int *)addr;
__asm__ __volatile__("": : :"memory");
return val;
}
static inline void writel(unsigned int value, volatile void *addr)
{
__asm__ __volatile__("": : :"memory");
*(volatile unsigned int *)addr = value;
__asm__ __volatile__("": : :"memory");
}
int main()
{
fd = open ("/dev/mem", O_RDWR | O_SYNC);
if(fd == 0)
{
DBG("open mem failed\n");
return -1;
}
iobase = mmap(NULL, 0x1000, PROT_READ|PROT_WRITE, MAP_SHARED, fd, 0x58002000);
if(iobase == MAP_FAILED)
{
DBG("iobase mmap failed\n");
ret = -1;
goto close_fd;
}
bcr0 = readl(iobase+FMC2_BCR(0));
...
writel(bcr0, iobase+FMC2_BCR(0));
...
}
But I guess I did not read the proper values of its registers, which are all 0x000030db. And if I try to write it, it did not change its value.
I had tried to do the same thing on STM32MP157D-EV1, but it could read the correct value and my writings did work.
Now I have to work on dk2 for some reasons, how can I configure it?
BTW, "cat /proc/iomem" will not print that range of mapped memory.
2024-05-17 3:20 AM
Hi @MapleLin
Maybe working on EV1 because the FMC is defined to be used for a NAND Flash.
Your enable of FMC is maybe not enough.
https://wiki.st.com/stm32mpu/wiki/FMC_device_tree_configuration#DT_configuration_-board_level-
See also clocking, if not used by any driver, Linux will not enable the IP clock.
https://wiki.st.com/stm32mpu/wiki/STM32MP15_clock_tree#Device_tree_2
Try also
cat /sys/kernel/debug/clk/clk_summary
Notice that FMC has multiple clocks (bus clock and a kernel clock). I think all should be enabled to access registers.
Regards
2024-05-21 12:03 AM
Hi @PatrickF .
As I am working with 4.19 version of linux kernel, it is not enough to enable fmc in device tree. The driver will quit at probe function when no nand device detected. The registers will be unmapped then, that is why I cannot access its registers.
Regards
2024-05-21 12:20 AM
Hi,
As you are in development phase, we strongly recommend to use latest ecosystem v5.x.
Otherwise, you could refer to wiki ecosystem v1 archive (https://wiki.st.com/stm32mpu-ecosystem-v1/wiki/Main_Page). Please note that this ecosystem is not supported anymore by ST.
Regards,
2024-05-23 10:02 PM
Hi.
I did realize that v4.x is not supported. But I have to do it for some special reasons. I will try using fmc with v5.15, and I have more questions. Below works are done under 4.19, but driver of 5.15 and 4.19 seems quiet similar, I guess they will be fit with 5.15.
1. I notice that there is no such a driver for fmc PSRAM/NOR, only a stm32_fmc2_nand.c file for nand driver. I think it is complex and difficult for me to write a PSRAM/NOR driver. So, I modified the nand driver so that it setup itself in psram mod, and not registered to mtd. And I could access nor memory range and registers in userspace then. But after I disable FMCEN, or trigger a reset with accessing RCC fmc reset register, I could not have fmc work again, even if I enabled FMCEN. (I configured it in sync mode and FMC_CLK didn't work.) Is there any other setup I missed?
2. I am wondering if it is possible to use MDMA to transfer data between fmc-nor/psram and ddr? As the reference manual RM0436 only mentioned DMA relative content in NAND mod. I don't have a real device connected with fmc currently, and I try to use dma transfer routine within nand driver, only an dma timeout happened.
Regards,
2024-05-24 1:01 AM
Hi,
I'm not SW expert, but starting latest ecosystem v5.x (I'm not sure for v4.x), you have the Linux PSRAM/NOR driver available (ebi.c).
see https://wiki.st.com/stm32mpu/wiki/FMC_internal_peripheral#Software_frameworks_and_drivers
and an example using an external SRAM like component (ksz8851, ethernet port on FMC) https://wiki.st.com/stm32mpu/wiki/FMC_device_tree_configuration#DT_configuration_of_the_external_bus_interface_controller_-board_level-
You have to seek only for a driver of your external device (or build your own if custom solution like FPGA).
If your external device is seen as memory mapped, I guess you could use MDMA for MEM2MEM transfert (using Linux DMA framework). Here I cannot help so much.
Regards,