2023-11-11 2:37 PM
Dear ST community,
I am currently trying to install an 8bit 8080 LCD , and i figured out that it needs FMC $ to be set up in devicetree in order to interface with it using DRM in Linux. i have the following device tree pinctrl nodes setup
fmc_pins_mx: fmc_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 0, AF12)>, /* FMC_D2 */
<STM32_PINMUX('D', 1, AF12)>, /* FMC_D3 */
<STM32_PINMUX('D', 4, AF12)>, /* FMC_NOE */
<STM32_PINMUX('D', 5, AF12)>, /* FMC_NWE */
<STM32_PINMUX('D', 7, AF12)>, /* FMC_NE1 */
<STM32_PINMUX('D', 14, AF12)>, /* FMC_D0 */
<STM32_PINMUX('D', 15, AF12)>, /* FMC_D1 */
<STM32_PINMUX('E', 7, AF12)>, /* FMC_D4 */
<STM32_PINMUX('E', 8, AF12)>, /* FMC_D5 */
<STM32_PINMUX('E', 9, AF12)>, /* FMC_D6 */
<STM32_PINMUX('E', 10, AF12)>, /* FMC_D7 */
<STM32_PINMUX('F', 0, AF12)>, /* FMC_A0 */
<STM32_PINMUX('G', 9, AF12)>; /* FMC_NE2 */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
};
fmc_sleep_pins_mx: fmc_sleep_mx-0 {
pins {
pinmux = <STM32_PINMUX('D', 0, ANALOG)>, /* FMC_D2 */
<STM32_PINMUX('D', 1, ANALOG)>, /* FMC_D3 */
<STM32_PINMUX('D', 4, ANALOG)>, /* FMC_NOE */
<STM32_PINMUX('D', 5, ANALOG)>, /* FMC_NWE */
<STM32_PINMUX('D', 7, ANALOG)>, /* FMC_NE1 */
<STM32_PINMUX('D', 14, ANALOG)>, /* FMC_D0 */
<STM32_PINMUX('D', 15, ANALOG)>, /* FMC_D1 */
<STM32_PINMUX('E', 7, ANALOG)>, /* FMC_D4 */
<STM32_PINMUX('E', 8, ANALOG)>, /* FMC_D5 */
<STM32_PINMUX('E', 9, ANALOG)>, /* FMC_D6 */
<STM32_PINMUX('E', 10, ANALOG)>, /* FMC_D7 */
<STM32_PINMUX('F', 0, ANALOG)>, /* FMC_A0 */
<STM32_PINMUX('G', 9, ANALOG)>; /* FMC_NE2 */
};
};
my problem is that i have pins from d4 to d7 are not accessible in my board, i am writing you to ask if there is a way to change the pins on AF12 and point them out to an other accessible pins?
(i have indeed tried cube-mx but it doesn't offer any other choice since this particular peripheral have no other alternate function options.)
Thank you
Solved! Go to Solution.
2023-11-12 11:37 PM
HI @iheb ,
unfortunately, there is no other options to route pins elsewhere.
Maybe you could use D15-D8 and define the FMC in 16-bits and make uses of upper byte only (in pinmux too). This will make D0-D7 not routed to any pins.
This is not available in CubeMx, pinmux section should be modified manually.
For SW point of view, might need to do tricky changes in the drivers (shift data and do 16-bits access), but maybe doable if you have no other options.
Regards.
2023-11-12 11:37 PM
HI @iheb ,
unfortunately, there is no other options to route pins elsewhere.
Maybe you could use D15-D8 and define the FMC in 16-bits and make uses of upper byte only (in pinmux too). This will make D0-D7 not routed to any pins.
This is not available in CubeMx, pinmux section should be modified manually.
For SW point of view, might need to do tricky changes in the drivers (shift data and do 16-bits access), but maybe doable if you have no other options.
Regards.