Regression in u-boot in Scarthgap branch
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-01-06 5:09 AM
Hi there,
The commit in question is rather huge and the general complaint is that commit message says nothing about the changes:
commit fd1832de6fb8c184904b64b6bb2e7df58d78d8f1
Author: Christophe Priouzeau <christophe.priouzeau@foss.st.com>
Date: Thu Oct 31 15:03:41 2024 +0100
U-BOOT: v2023.10-stm32mp-r1
Change-Id: Ic24598b586631a0a3f7dae9b54b513ff87ad461a
Signed-off-by: Christophe Priouzeau <christophe.priouzeau@foss.st.com>
But only this particular snippet causes problems:
+# do not populate image directory during install
+do_install[noexec] = "1"
Why was the assumption that it shouldn't be executed? In my case I use the default environment, which is supposed to be installed by the do_install task.
Labels:
- Labels:
-
OpenSTLinux
-
U-Boot
-
Yocto
0 REPLIES 0