qt-wpe-simple-browser error with wpewebkit-qtwpe-qml-plugin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-14 2:52 AM
Hi
i try to install qt-wpe-simple-browser on my board but it fails with error wpewebkit-qtwpe-qml-plugin.
ERROR: st-image-qt-1.0-r0 do_rootfs: Unable to install packages. Command '/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-qt/1.0-r0/recipe-sysroot-native/usr/bin/apt-get install --allow-downgrades --allow-remove-essential --allow-change-held-packages --allow-unauthenticated --no-remove apt cog dpkg packagegroup-base-extended packagegroup-core-boot packagegroup-core-eclipse-debug packagegroup-core-ssh-dropbear packagegroup-core-tools-profile packagegroup-framework-core packagegroup-framework-core-base packagegroup-framework-core-extra packagegroup-framework-tools packagegroup-framework-tools-base packagegroup-optee-core packagegroup-optee-test packagegroup-st-demo packagegroup-x-linux-qt psplash-drm qt-wpe-simple-browser qtbase-plugins qtwayland-plugins resize-helper run-postinsts wpewebkit wpewebkit-qtwpe-qml-plugin' returned 100:
Reading package lists...
Building dependency tree...
Reading state information...
Package wpewebkit-qtwpe-qml-plugin is not available, but is referred to by another package.
This may mean that the package is missing, has been obsoleted, or
is only available from another source
E: Package 'wpewebkit-qtwpe-qml-plugin' has no installation candidate
ERROR: Logfile of failure stored in: /home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/st-image-qt/1.0-r0/temp/log.do_rootfs.18362
ERROR: Task (/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-st/meta-st-x-linux-qt/recipes-st/images/st-image-qt.bb:do_rootfs) failed with exit code '1'
NOTE: Tasks Summary: Attempted 8801 tasks of which 8774 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 2 seconds
Summary: 1 task failed:
/home/md/Workspace/Demo_file_fr/MPU_EDS_V1.0/layers/meta-st/meta-st-x-linux-qt/recipes-st/images/st-image-qt.bb:do_rootfs
Summary: There were 3 WARNING messages.
Summary: There was 1 ERROR message, returning a non-zero exit code.
- Labels:
-
STM32MP15 Lines
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-18 7:22 AM
Qt-wpe is no more supported.
You can try a PyQt5 based browser.
If you plan to browse only in a kiosk mode, you can try the Qt official example:
https://doc.qt.io/qt-5/qtwebengine-webengine-quicknanobrowser-example.html
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-10-19 4:32 AM
Hi @PPAGE.13
Thanks for your respone,
Actually i can not use the https://doc.qt.io/qt-5/qtwebengine-webengine-quicknanobrowser-example.html
this one , because of the Qtwebengine , in yocto layers , meta- python2 , no more support or branch in mickledore,
So i moved on yocto 23.06.21(v5.0.1) , where i download the starter package and i installed the python3-pyqt5,
where i successfully displayed the web-browser , but it issueing with the browser playing video , also i try to play the video using the GST play , but fails,
so as of now i am using the yocto 23.06.21 version , and debugging the GStreamer1.0, i am using the distribution package.
No more support on latest version , there is many error and bugs, with wpewebkit , qtwebengine,qt-wpe, and many more ,