2024-08-06 10:35 PM
how to setup qt creater application for STM32MP157f-Dk2 board , and where is the location of the toolchain location and how to setup qt version .
Solved! Go to Solution.
2024-08-09 05:35 AM
please help me out from image 6 why this happen
please
2024-08-09 05:47 AM
Hello,
very good, your environment looks ready to develop your application.
I suggest anyway you run an existing "hello world" example before doing your own one.
Please look at Qt documentation, like this one: https://doc.qt.io/qt-5/qml-tutorial1.html
And let me know if compilation and execution is fine.
BR,
Philippe.
2024-08-10 12:26 AM
hi @PPAGE.13
please help me out this, it is showing warning.
and i run the hello world application(Hello_World) without sudo it is working but , when i use the application with sudo it will give the error as like a warning.
2024-08-20 03:54 AM
Hi,
please go to following chapter for more details
"9.6. Configure the STM3 MPU Kit" in
https://wiki.st.com/stm32mpu/wiki/X-LINUX-QT_Expansion_Package
To summarize: the 2 variables below must be set in Qt Creator "Run" Qt configuration when you launch test from the host:
XDG_RUNTIME_DIR=/run/user/1000 QT_QPA_PLATFORM=wayland
When you execute the test from the target, these variables are already set by default.
BR,
Philippe.