2019-03-23 3:58 PM
I am trying to add a kernel module for USB serial devices following: https://askubuntu.com/questions/168279/how-do-i-build-a-single-in-tree-kernel-module
In order to build just the module, not a completely new kernel , I would need the Module.symvers file. Any idea where to find it?
Solved! Go to Solution.
2019-04-08 6:56 AM
Yocto build is not providing this file by default, so ST is not providing it in its delivery. So you will need to build the kernel to have it (but I understand this is what you don't want to do ...).
We think the safer and generic way to proceed is to make the menuconfig and rebuild the kernel with this config. This is the only way to make sure all the dependencies are well managed.
OpenSTLinux kernel is not big and you will need only 10/15 minutes to build it from scratch with the Developer package (see the link above).
2019-03-28 8:20 AM
Hi,
Did you have a look to wiki article here ?
https://wiki.st.com/stm32mpu/wiki/How_to_cross-compile_with_the_Developer_Package
Section 6 Modifying/adding an external Linux kernel module might give you some clue
Olivier
2019-03-30 2:32 PM
Yes, I have seen that. This is what I am doing, but without Module.symvers you need to force insmod the resulting kernel modules. Without the file, a complete re-built of the kernel is required.
2019-04-08 6:56 AM
Yocto build is not providing this file by default, so ST is not providing it in its delivery. So you will need to build the kernel to have it (but I understand this is what you don't want to do ...).
We think the safer and generic way to proceed is to make the menuconfig and rebuild the kernel with this config. This is the only way to make sure all the dependencies are well managed.
OpenSTLinux kernel is not big and you will need only 10/15 minutes to build it from scratch with the Developer package (see the link above).