2022-12-17 02:13 AM
2022-12-17 08:14 AM
Hello @AFard.1 ,
For low performances and bad user experience reasons, ST chose to not support Android on this platform anymore.
Kind regards,
Erwan.
2022-12-17 08:14 AM
Hello @AFard.1 ,
For low performances and bad user experience reasons, ST chose to not support Android on this platform anymore.
Kind regards,
Erwan.
2022-12-17 11:41 PM
Hello Erwan,
thank you very much for the quick reply,
Actually we are developing a custom hardware based on same soc STM32MP157 Arm®-based dual Cortex®-A7 32 bits + Cortex®-M4 as stm32mp157a-dk1 dev board , I want to prepare the android environment for the dev board before doing the bring up of our custom hardware, do you have any suggestions please?
best regards
ahmed fardi
2022-12-22 06:45 AM
Hello @AFard.1 ,
As I said, we will not be able to provide a lot of support on Android. The only little tips that we can give are the ones below:
Moreover, for security reason, I am not sure that you will be able to boot Android on stm32mp157a. Only c and f should be usable.
I hope that it will help you a little bit in your bring up process.
As mentioned on the wiki, if you need more support, you can contact our partner Witekio.
Kind regards,
Erwan.
2023-03-13 02:30 PM
Hello Erwan , we switched to use the eval board STM32MP157f-EV1 , based on it w started the hardware dev .
I downloaded the st-android-11.0.0-2021-01-29 android soft , and flashed the baord , the switches are configured to boot from emmc , the startup of android system is ok but without screen , the dispaly is white , the tactil working fine i can see by the logcat all the services are fine even the ST laucher com.stmicroelectronics.stlauncher.
Any help please ? , i tried to build locally a soft , flashed to sdcard but i faced the same problem on the dispaly .
I attached the full log here