2025-01-07 12:41 AM
Hello,
for flashing my STM32MP135F-DK board I am using STM_Programmer_CLI with my .tsv file. Example command and my tsv file:
sudo ./STM32_Programmer_CLI -c port=usb1 -w path/to/my.tsv
Is there a way to explicitly set partitions UUID for rootfs-a and rootfs-b during flashing?
I've noticed that when I name a partition with rootfs then it gets UUID of e91c4e10-16e6-4c0e-bd0e-77becf4a3582, as described in the wiki . But when having rootfs-a and rootfs-b, then those partitions get some other UUID, and the boot stops because rootfs UUID is not e91c4e10-16e6-4c0e-bd0e-77becf4a3582.
I need the rootfs-a and rootfs-b UUIDs to be constant, to manage FW upgrades.
2025-01-09 08:42 AM
Hello @mmichala,
I guess you use meta-st-ota layer : to avoid that problem, I would recommand to flash the image into the sdcard with create_sdcard_from_flashlayout.sh script available in the layer, where bootfs-b UUID is managed.
Neverthless, I take the point to bring rootfs-b support in CubeProgrammer (and also rootfs-a/b, vendorfs-a/b...).
BR,
Christophe
2025-01-10 03:46 AM
When using STM32MP135F-DK I have a possibility to take SD card out and plug it into host PC to use create_sdcard_from_flashlayout.sh script and 'dd' to populate it.
But STM32MP135F-DK is only my test/development board, and for production I will be using another hardware with eMMC. That's why I've already used STM_Programmer_CLI method even for STM32MP135F-DK.
Now there is a problem for me, because the development time is ticking and I can't get OTA working. Previously I was using Yocto kirkstone, and meta-st-ota for kirkstone was using partition labels, which was working fine when migrated to my project.
But I had to upgrade Yocto from Kirkstone to Scarthgap, and that's why I also updated meta-st-ota.
May I ask you @Christophe Guibout , when approximately will this support in CubeProgrammer be ready?
Best Regards
Mateusz
2025-01-10 06:02 AM
Hello @mmichala,
Instead of configuring an hardcoded PARTUUID for rootfs-b, I think it's better to read it at runtime (with blkid) in order to update the kernel command line accordingly.
I updated the meta-st-ota layer with this correction.
BR,
Christophe