Hello, I want to enable SPI4 but just get a timeout. My SOM is based on STM32MP157, use Linux 5.10 Main line. I connected a logic analyser and see the pins are set to high a soon linux was booted. I dont see any clock impulses.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-02-22 12:30 AM
My device tree:
spi4_pins_csa: spi4-0 {
pins {
pinmux = <STM32_PINMUX('E', 12, AF5)>, /* SPI4_SCK */
<STM32_PINMUX('E', 14, AF5)>; /* SPI4_MOSI */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('E', 13, AF5)>; /* SPI4_MISO */
};
};
&spi4 {
pinctrl-names = "default";
pinctrl-0 = <&spi4_pins_csa>;
cs-gpios = <GPIO_CO_CS GPIO_ACTIVE_LOW>;
status = "okay";
spidev@0{
compatible = "spidev";
reg = <0>;
spi-max-frequency = <4000000>;
};
};
The output:
root@apollo-e2412:~# spidev_test -D /dev/spidev1.0
spi mode: 0x4
bits per word: 8
max speed: 500000 Hz (500 kHz)
[ 609.925039] spidev spi1.0: SPI transfer timed out
[ 609.928391] spi_master spi1: failed to transfer one message from queue
can't send spi message: Connection timed out
Aborted
Labels:
- Labels:
-
SPI
-
STM32MP15 Lines
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-11-09 10:53 AM
Any luck with this? I'm hitting a similar issue with the SPI busses on STM32MP157 with the mainline and the ST kernel 5.10.x kernel.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-11-09 1:17 PM
Hi,
I had a slightly different issue with sdmmc1 where it would not initialise without defining the "sleep" pins. I have had success with SPI5 on an STM32MP135 like this:
&pinctrl {
spi5_pins_mx: spi5-1 {
pins1 {
pinmux = <STM32_PINMUX('G', 10, AF5)>, /* SPI4_SCK */
<STM32_PINMUX('H', 12, AF5)>; /* SPI4_MOSI */
bias-disable;
drive-push-pull;
slew-rate = <1>;
};
pins2 {
pinmux = <STM32_PINMUX('G', 8, AF5)>; /* SPI4_MISO */
bias-disable;
};
};
spi5_sleep_pins_mx: spi5-sleep-1 {
pins {
pinmux = <STM32_PINMUX('G', 10, ANALOG)>, /* SPI4_SCK */
<STM32_PINMUX('G', 8, ANALOG)>, /* SPI4_MISO */
<STM32_PINMUX('H', 12, ANALOG)>; /* SPI4_MOSI */
};
};
};
...
&spi5 {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&spi5_pins_mx>;
pinctrl-1 = <&spi5_sleep_pins_mx>;
cs-gpios= <&gpioe 8 GPIO_ACTIVE_LOW>; //PE8 = CS for WiFi
status = "okay";
...
};
View more
Maybe this is related to your problem? Good luck.
Tom