2024-08-13 8:11 PM
The Linux version I am using is 6.1.28, and my power management is a discrete component. "VDD_CORE" is actually 1.212V, and in the device tree it looks like this:
vddcore: regulator-vddcore {
compatible = "regulator-fixed";
regulator-name = "vddcore";
regulator-min-microvolt = <1200000>;
regulator-max-microvolt = <1350000>;
regulator-always-on;
regulator-boot-on;
};
If I follow the above settings, my "/sys/devices/system/cpu/cpufreq/" will be empty, but if I change the 1200000 in "regulator min microvolt=<1200000>;" to 1350000, it will be normal. Why is this?
Solved! Go to Solution.
2024-09-27 1:57 AM
Hi @zengyixiang
Sorry this is not clear , if you have a static discrete VDD_CORE to 1.2V you can't support the 1.35 / 800Mhz opp mode.
You might put 1200000 in both min / max and check opp_table to let only a single conf.
How to change the CPU frequency - stm32mpu
Olivier
2024-09-27 1:57 AM
Hi @zengyixiang
Sorry this is not clear , if you have a static discrete VDD_CORE to 1.2V you can't support the 1.35 / 800Mhz opp mode.
You might put 1200000 in both min / max and check opp_table to let only a single conf.
How to change the CPU frequency - stm32mpu
Olivier