2020-07-21 06:28 PM
Hi,I execute the following commands according to the wiki:(I am sure accept the EULA)
PC $> DISTRO=openstlinux-eglfs MACHINE=stm32mp1 source layers/meta-st/scripts/envsetup.sh
PC $> bitbake st-example-image-qt
The following is part of the terminal output :(bitbake st-example-image-qt)
NOTE: Executing Tasks
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: oe_runmake failed
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: Execution of '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.12684' failed with exit code 1:
make: Entering directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found. Stop.
make: Leaving directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
WARNING: exit code 1 from a shell command.
ERROR: Logfile of failure stored in: ../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_compile.12684
Log data follows:
| DEBUG: Executing python function tfaconfig_env
| DEBUG: Python function tfaconfig_env finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 8 CROSS_COMPILE=arm-ostl-linux-gnueabi- DEBUG=1 LOG_LEVEL=40 PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 STM32MP_SPI_NOR=1 STM32MP_RAW_NAND=1 STM32MP_SPI_NAND=1 -C ../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/git DTB_FILE_NAME=stm32mp157a-dk1.dtb BUILD_PLAT=../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted AARCH32_SP=sp_min
| make: Entering directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found. Stop.
| make: Leaving directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| ERROR: oe_runmake failed
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.12684' failed with exit code 1:
| make: Entering directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found. Stop.
| make: Leaving directory '../openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxeglfs-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| WARNING: exit code 1 from a shell command.
|
ERROR: Task (../openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 4867 tasks of which 4531 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 10 seconds
Summary: 1 task failed:
../openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.
Solved! Go to Solution.
2020-07-22 12:07 AM
Hi @One&Zero
looks similar to issue in this post :
Fixed by doing bitbake -c cleanall tf-a-stm32mp and relaunch.
Hope it help
Olivier
2020-07-22 12:07 AM
Hi @One&Zero
looks similar to issue in this post :
Fixed by doing bitbake -c cleanall tf-a-stm32mp and relaunch.
Hope it help
Olivier
2020-07-22 05:35 PM
Thank you @OlivierG (ST Employee) it worked!