Skip to main content
NRosa.1
Associate II
Jul 20, 2020 2:53 PM UTC
Solved

Error in building the OpenSTLinux distribution

I'm trying to build the standard st-image-weston image following this guide:

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package

After starting the build with

bitbake st-image-weston

When it reaches around the 68% of the process I get the following error:

ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: oe_runmake failed
ERROR: tf-a-stm32mp-2.2.r1-r0 do_compile: Execution of '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.21431' failed with exit code 1:
make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found. Stop.
make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
WARNING: exit code 1 from a shell command.
 
ERROR: Logfile of failure stored in: /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_compile.21431
Log data follows:
| DEBUG: Executing python function tfaconfig_env
| DEBUG: Python function tfaconfig_env finished
| DEBUG: Executing shell function do_compile
| NOTE: make -j 4 CROSS_COMPILE=arm-ostl-linux-gnueabi- DEBUG=1 LOG_LEVEL=40 PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 STM32MP_SPI_NOR=1 STM32MP_RAW_NAND=1 STM32MP_SPI_NAND=1 -C /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/git DTB_FILE_NAME=stm32mp157a-dk1.dtb BUILD_PLAT=/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted AARCH32_SP=sp_min
| ERROR: oe_runmake failed
| make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found. Stop.
| make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| WARNING: exit code 1 from a shell command.
| ERROR: Execution of '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.21431' failed with exit code 1:
| make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| make: *** No targets specified and no makefile found. Stop.
| make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
| WARNING: exit code 1 from a shell command.
| 
ERROR: Task (/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/layers/meta-st/meta-st-stm32mp/recipes-bsp/trusted-firmware-a/tf-a-stm32mp_2.2.bb:do_compile) failed with exit code '1'

I haven't added anything besides the cloned repository.

Am I doing something wrong?

This topic has been closed for replies.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Jul 21, 2020 7:33 AM UTC

Please try bitbake -c cleanall tf-a-stm32mp and relaunch.

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

13 replies

Olivier GALLIEN
ST Technical Moderator
Jul 20, 2020 2:58 PM UTC

Hi @NRosa.1​ 

I notice you are using latest 5.4-Dunfell/V2.0 version.

Some extra package are requested compare to previous 4.19-Thud / V1.2 on Host side.

Please check carefully this section :

https://wiki.st.com/stm32mpu/wiki/PC_prerequisites#Install_extra_packages

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NRosa.1
NRosa.1Author
Associate II
Jul 20, 2020 3:11 PM UTC

Hi @Community member​ ,

I rechecked all of the additional software required and it appears to me that everything is already installed.

Could anything else be the cause of the error?

Olivier GALLIEN
ST Technical Moderator
Jul 20, 2020 3:31 PM UTC

Hi,

>> make: *** No targets specified and no makefile found. Stop.

This is strange.

What is your configuration ( machine, distro ) ?

Thx

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NRosa.1
NRosa.1Author
Associate II
Jul 20, 2020 3:36 PM UTC

I'm using the standard configuration, that means DISTRO=openstlinux-weston MACHINE=stm32mp1.

As for the OS for the compilation I'm using a Ubuntu 18.04.3 virtual machine using VirtualBox on a Windows 10 enviroment.

Olivier GALLIEN
ST Technical Moderator
Jul 20, 2020 4:01 PM UTC

Hi @NRosa.1​ 

you are working in a fully validated configuration/environment at our end.

Did you have a look to the mentionned log :

Logfile of failure stored in: /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/log.do_compile.21431

Does it contain useful info ?

Are you sure the error at do_compile is the first one ? do_fetch succeed ?

Can you make a try of :

bitbake tf-a-stm32mp

Thanks

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NRosa.1
NRosa.1Author
Associate II
Jul 21, 2020 7:08 AM UTC

Good morning @Community member​ ,

The content of the log file is basically the same as the error message in the console, and it is the following

DEBUG: Executing python function tfaconfig_env
DEBUG: Python function tfaconfig_env finished
DEBUG: Executing shell function do_compile
NOTE: make -j 4 CROSS_COMPILE=arm-ostl-linux-gnueabi- DEBUG=1 LOG_LEVEL=40 PLAT=stm32mp1 ARCH=aarch32 ARM_ARCH_MAJOR=7 STM32MP_SDMMC=1 STM32MP_EMMC=1 STM32MP_SPI_NOR=1 STM32MP_RAW_NAND=1 STM32MP_SPI_NAND=1 -C /home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/git DTB_FILE_NAME=stm32mp157a-dk1.dtb BUILD_PLAT=/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/build/trusted AARCH32_SP=sp_min
make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found. Stop.
make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
ERROR: oe_runmake failed
WARNING: exit code 1 from a shell command.
ERROR: Execution of '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work/stm32mp1-ostl-linux-gnueabi/tf-a-stm32mp/2.2.r1-r0/temp/run.do_compile.2316' failed with exit code 1:
make: Entering directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
make: *** No targets specified and no makefile found. Stop.
make: Leaving directory '/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source'
WARNING: exit code 1 from a shell command.

So unfortunately not very useful.

I suppose that do_fetch had succeeded, but right now it skips directly to do_compile so I'm not sure how can I verify that.

As you can imagine, trying to run bitbake tf-a-stm32mp results in the same exact error in the do_compile.

By the way thanks for all the help and the quick responses.

Noah

Olivier GALLIEN
ST Technical Moderator
Jul 21, 2020 7:19 AM UTC

Hi @NRosa.1​ 

>> I suppose that do_fetch had succeeded, but right now it skips directly to do_compile so I'm not sure how can I verify that.

You should find tf-a sources in "/home/osboxes/openstlinux-5.4-dunfell-mp1-20-06-24/build-openstlinuxweston-stm32mp1/tmp-glibc/work-shared/stm32mp1/tfa-source"

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Olivier GALLIEN
Olivier GALLIENBest answer
ST Technical Moderator
Jul 21, 2020 7:33 AM UTC

Please try bitbake -c cleanall tf-a-stm32mp and relaunch.

Hope it help

Olivier

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
NRosa.1
NRosa.1Author
Associate II
Jul 21, 2020 7:49 AM UTC

Thank you @Community member​ it worked!

It seems a bit strange to me since I already tried to clean the whole st-image-weston recipe and it didn't work. Is there a difference between cleaning everything or the single recipe?

Thanks again and have a good day.

NRosa.1
NRosa.1Author
Associate II
Jul 21, 2020 7:40 AM UTC

The folder is empty so it seems to have failed?

Is it possible that do_fetch and do_compile execute in the wrong order?