cancel
Showing results for 
Search instead for 
Did you mean: 

After a Linux Kernel Rebuild I see only one CPU

frenchie68
Associate II

Hello,

I am using the STM32MP157F-DK2 and recently went through a textbook rebuild of the Linux kernel, the modules and the gcnano driver (for GL support). All is well and yet, I see only one of the two CPUS. dmesg tells me the following:

[   0.000000] ------------[ cut here ]------------

[   0.000000] WARNING: CPU: 0 PID: 0 at arch/arm/kernel/devtree.c:148 arm_dt_init_cpu_maps+0x168/0x250

[   0.000000] DT /cpu 2 nodes greater than max cores 1, capping them

[   0.000000] Modules linked in:

[   0.000000] CPU: 0 PID: 0 Comm: swapper Not tainted 5.15.67 #1

[   0.000000] Hardware name: STM32 (Device Tree Support)

[   0.000000] [<c010e8ec>] (unwind_backtrace) from [<c010c158>] (show_stack+0x10/0x14)

[   0.000000] [<c010c158>] (show_stack) from [<c0122404>] (__warn+0xec/0x148)

[   0.000000] [<c0122404>] (__warn) from [<c0c33034>] (warn_slowpath_fmt+0x78/0xac)

[   0.000000] [<c0c33034>] (warn_slowpath_fmt) from [<c1105094>] (arm_dt_init_cpu_maps+0x168/0x250)

[   0.000000] [<c1105094>] (arm_dt_init_cpu_maps) from [<c1104b1c>] (setup_arch+0x13c/0x170)

[   0.000000] [<c1104b1c>] (setup_arch) from [<c1100c2c>] (start_kernel+0x6c/0x61c)

[   0.000000] [<c1100c2c>] (start_kernel) from [<00000000>] (0x0)

[   0.000000] ---[ end trace 58996bc4bee07162 ]---

How do I reconfigure the system to have both CPUs active?

Thanks in advance.

Francois

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bernard PUEL
ST Employee

Hello,

fragment-06-smp-config has to be applied only in case of single cpu use case. It is not clearly mentioned in the README file, and therefore, this is under correction (README file update).

fragment-05-signature.config as well is only required for secure boot.

So probably in your case, you need to apply only the fragments 03 and 04 (on top of the kernel fragments already set).

Hope it is clear.

View solution in original post

6 REPLIES 6
frenchie68
Associate II

According to https://bootlin.com/blog/building-a-linux-system-for-the-stm32mp1-basic-system/ (buildroot based guidelines for the STM32MP157F-DK2), I should have SMP displayed before PREEMT when u-boot transfers control to he Linux kernel and I don't.

More research is needed to straighten this out.

frenchie68
Associate II

At some point (git checkout of the kernel source tree), fragment-06-smp.config surfaced and I applied it dutifully. It appears to be meant to disable the SMP feature altogether:

# CONFIG_SMP is not set

Any particular reason for this?

frenchie68
Associate II

It turns out that the developer package supplies fragment-06-smp-config as in en.SOURCES-stm32mp1-openstlinux-5.15-yocto-kirkstone-mp1-v22.11.23.tar. I'd really like to hear someone from ST with an official position with respect to SMP support on the SMT32MP157.

Bernard PUEL
ST Employee

Hello,

fragment-06-smp-config has to be applied only in case of single cpu use case. It is not clearly mentioned in the README file, and therefore, this is under correction (README file update).

fragment-05-signature.config as well is only required for secure boot.

So probably in your case, you need to apply only the fragments 03 and 04 (on top of the kernel fragments already set).

Hope it is clear.

Yes it is quite clear, thank you Bernard. I suspected that much since I came across boot logs dating back from September last year that indicated that SMP was originally enabled.

frenchie68
Associate II

The system now comes up as SMP.

root@stm32mp157:~# uname -a

Linux stm32mp157 5.15.67 #2 SMP PREEMPT Mon Feb 27 19:22:34 CET 2023 armv7l armv7l armv7l GNU/Linux

Now to rebuild the gcnano driver.