cancel
Showing results for 
Search instead for 
Did you mean: 

Why Flashing the FSBL Failed?

SCho.3
Associate

I have a DK2 board.

Downloading FSBL image for EV1 board to DK2 board through USB port on DFU by the STM32CubeProgrammer fails. Both boards use the STM32MP157C chip, but I don't understand why the download fails.

Can anyone explain the reason or principle?

1 REPLY 1
Olivier GALLIEN
ST Employee

Hi @SCho.3​ 

Are you using complete TSV file from EV1 ?

You need a custom one specifying DK2 fsbl1-boot and ssbl-boot for partition 0x1 and 0x3 ( they will be executed on DK2 for flash procedure)

Other partition kept with EV1 image partitions

Hope it help

Olivier

Olivier GALLIEN
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.