2019-11-04 11:38 PM
Hello,
I am working on the evaluation board STM32MP157CDk2
I am trying to add my code in the main method while loop in order to toogle pins.
I added the following code:
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_TogglePin(atoi(1), GPIO_PIN_11);
HAL_Delay(100);
HAL_GPIO_TogglePin(atoi(0), GPIO_PIN_11);
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
I have two questions.
1) I get the following error (attached) after i choose target and then program chip
2) I am connected through usb and UART in the eclipe, am using the system work bench as an IDE. Is there something to do before doing the build for connecting with the device in a special way?. I can see in the console that i am connected to the board. and Eclipse shows the message at the buttom (Serial Console in use).
I am new to this. I appreciate your help alot
Best Regards
Solved! Go to Solution.
2019-11-06 12:48 AM
Don't use "run" but go to "Debug" and then look for "ST’s STM32 MPU Debugging" configuration.
You are going to want to read this: https://www.openstm32.org/Using%2BSTM32-CoPro-MPU%2Bplugin
2019-11-05 2:32 AM
You should use GPIOA (point to PA11 in your case) instead atoi(1) and atoi(0)
Also, add delay function after second toggle or remove line 6 at all.
2019-11-05 4:45 AM
I did but that is not the problem. It seams like its not finding some config file, i do not know if that the config file of the OCD and where to find it and where to define it in the program.
2019-11-05 6:33 PM
What IDE are you using? The error message clearly states that you don't have the OpenOCP config file.
2019-11-06 12:39 AM
I am using the System Workbench. i configured the OpenOCD. through run-> external tools-> as seen in the attachment. and the openocd now is configured, it is just listening on port 333 for the gdb. but after i configured the gdb. I have the following message:
Open On-Chip Debugger 0.10.0+dev-01124-gbfb41e6 (2018-11-16-15:00)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.org/doc/doxygen/bugs.html
cortex_a interrupt mask on
cortex_a interrupt mask on
cortex_a domain access control fixup on
cortex_a domain access control fixup on
3333
none separate
adapter speed: 5000 kHz
adapter_nsrst_assert_width: 200
adapter_nsrst_delay: 200
none srst_pulls_trst
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : STLINK V2J34S25 (API v2) VID:PID 0483:3752
Info : using stlink api v2
Info : Target voltage: 3.257143
Info : clock speed 5000 kHz
Info : SRST line released
Info : stlink_connect(connect)
Info : SWD DPIDR 0x6ba02477
Info : stm32mp15x.cpu0: hardware has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : Listening on port 3334 for gdb connections
Info : Listening on port 3333 for gdb connections
srst_only srst_pulls_trst srst_gates_jtag srst_open_drain connect_deassert_srst
Info : accepting 'gdb' connection on tcp/3333
Info : stm32mp15x.cpu2: hardware has 6 breakpoints, 4 watchpoints
target halted due to debug-request, current mode: Thread
xPSR: 0x01000000 pc: 0x00000008 msp: 0x00000100
Info : New GDB Connection: 1, Target stm32mp15x.cpu2, state: halted
ap 0 selected, csw 0x10006000
Info : SRST line asserted
Info : SRST line released
Info : stlink_connect(connect)
Info : SWD DPIDR 0x6ba02477
Error: timed out while waiting for target halted
Info : stm32mp15x.cpu0 rev 5, partnum c07, arch f, variant 0, implementor 41
Info : stm32mp15x.cpu0 cluster 0 core 0 multi core
target halted in ARM state due to debug-request, current mode: Supervisor
cpsr: 0x800001d3 pc: 0x000092a0
MMU: disabled, D-Cache: disabled, I-Cache: disabled
ap 0 selected, csw 0x10006000
pc (/32): 0x000092A0
Info : Deferring arp_examine of stm32mp15x.cpu1
Info : Use arp_examine command to examine it manually!
Info : stm32mp15x.cpu1: hardware has 6 breakpoints, 4 watchpoints
Info : stm32mp15x.cpu1 rev 5, partnum c07, arch f, variant 0, implementor 41
Info : stm32mp15x.cpu1 cluster 0 core 1 multi core
target halted in Thumb state due to debug-request, current mode: Supervisor
cpsr: 0x800001f3 pc: 0x0000060e
MMU: disabled, D-Cache: disabled, I-Cache: enabled
Info : Deferring arp_examine of stm32mp15x.cpu2
Info : Use arp_examine command to examine it manually!
Info : Deferring arp_examine of stm32mp15x.ap2
Info : Use arp_examine command to examine it manually!
Error: Target not examined yet
embedded:startup.tcl:24: Error:
in procedure 'stm32mp15x.cpu0' called at file "target/stm32mp15x.cfg", line 185
in procedure 'ocd_bouncer'
at file "embedded:startup.tcl", line 24
Error: Target not examined yet
embedded:startup.tcl:24: Error:
in procedure 'stm32mp15x.cpu0' called at file "target/stm32mp15x.cfg", line 185
in procedure 'ocd_bouncer'
at file "embedded:startup.tcl", line 24
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
Error: Target not examined yet
ap 0 selected, csw 0x10006000
Any idea where is this coming from?
Regards
2019-11-06 12:48 AM
Don't use "run" but go to "Debug" and then look for "ST’s STM32 MPU Debugging" configuration.
You are going to want to read this: https://www.openstm32.org/Using%2BSTM32-CoPro-MPU%2Bplugin
2019-11-06 1:12 AM
Ok, I ran it through the ST’s STM32 MPU Debugging and it connected to the IP address to the board and now i can see the root@stm32mp1.
but i added that code. inside the while loop of the main.c
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_11);
HAL_Delay(500);
HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_11);
I cannot see any difference in the blinking of the PIN11 which is the blue LED on the board. also, evrytime i change the HAL delay, do i have to start debugging the board again or is it real time?
Thanks in Advance
2019-11-06 1:31 AM
GPIOA Pin 11 is NOT an LED pin. Please read the document before doing anything: https://www.st.com/content/ccc/resource/technical/document/user_manual/group1/d6/59/df/e0/8f/e7/45/8f/DM00591354/files/DM00591354.pdf/jcr:content/translations/en.DM00591354.pdf
Also, your code basically double-toggling the pin without delay, effectively making it nothing at all. Add a delay as the first comment says.
Lastly there is no C debugging tool on earth that automatically update code changes in real time.
2019-11-06 1:43 AM
Ok. Thanks i understand that now. Sorry because i am new to this, just wanted to check if i can change any blinking LED while i am connected to the board. but struggling with that
2019-11-06 1:48 AM
No worries, just try with GPIOH and GPIO_PIN_11, and delete the last HAL_GPIO_TogglePin. You will see an orange LED blinking =)