2025-01-04 11:53 AM - edited 2025-01-04 12:15 PM
I have two STM32MP157C-DK2 dev boards, they still have the demo software on it.
They collected a lot of dust, over the past years.
The problem is the 3d cube demo slowing down after days.
After a reset it is fast again. Perhaps a memory leak?
Because it needs a reset every day or maybe every hour, I never was willing to start developing software on it.
I'm cleaning up, and I am about to throw these kits in the trashbin.
But, what's the undelying problem? Is there a solution to keep de kits running stable and at full speed anyway?
2025-01-06 12:29 AM
Hi @Jack3
I will give a try on my side with latest ecosystem on latest board STM32MP157F-DK2.
Which version of SW ecosystem or Linux kernel version you have on the board ?
Did you try to put the latest ecosystem SW on the board ?
I assume the one delivered on SD-Card with this board is very old and largely updated meanwhile.
Regards.
2025-01-06 11:38 PM
I would check what the "top" and "free" commands say in both instances.
2025-01-06 11:45 PM
Hi,
After about 1 day running the 3D demo on STM32MP157F-DK2 with latest ecosystem 6.x, I did not see any visible slow down not any significant change within 'top' results.
I keep it running.
Regards,