2023-06-23 12:33 PM
Not sure if this is the right place to write this, but I cannot help to write:
- STLINK-V3PWR is a great tool.
- I wish it had an external power input other than USB-C. It may be common in some computer setups, but powered USB ports might be challenging to find, and hubs with powered ports are not easy to find. The power specs of the ports are also not always given. An external power input would solve this for good. By chance, the USB hub I purchased a while ago for a different purpose has charging data ports, which helped in this case.
- I did not check the recent boards, and I don't know if the product design thinking is that this is going to be used on customer-designed boards with debug connectors. However, not all boards have such connectors, and the debug pins on STLINK-V3PWR are not exposed. By chance, I have an adapter/break-out board for ARM10 and I used that but I think the product should have either a break-out board included or even better these pins (SWD) should also be exposed like the bridge interface.
2023-10-21 10:53 AM
Some feedback from me: