2024-05-08 08:55 PM
I'm attempting to run an OP-TEE Trusted Application on the STM32MP157F-DK2 running OpenST Linux version stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21. I've followed the guides here and here, but both end up producing the following error when attempting to run the application:
TEEC_Opensession failed with code 0xffff0008 origin 0x3
What could be causing this problem? I'm running a fresh install of OpenST Linux and haven't made any modifications to the system other than those required to get the example running.
Solved! Go to Solution.
2024-05-13 02:29 PM
2024-05-13 02:29 PM