2023-02-12 02:48 AM
Hi @OlivierK ,
I am using openstlinux ecosystem release v3.1.1 and trying to use secure boot feature with yocto and as per https://wiki.st.com/stm32mpu-ecosystem-v3/wiki/TF-A_overview we need to set "TRUSTED_BOARD_BOOT=1".
We need use "TF_A_SIGN_ENABLE=1" to use "TRUSTED_BOARD_BOOT=1" in meta-st-stm32mp.
If TF_A_SIGN_ENABLE=1 then FIP_SIGN_ENABLE will get set as per ecosystem release v3.1.1 and which force to set FIP_SIGN_KEY_EXTERNAL FIP_SIGN_KEY FIP_SIGN_KEY_PASS and TF_A_SIGN_ENABLE as per https://wiki.st.com/stm32mpu/wiki/How_to_perform_Secure_Boot_from_Distribution_package.
I do not want set FIP_SIGN_KEY_EXTERNAL FIP_SIGN_KEY FIP_SIGN_KEY_PASS at the time of build and want set after build seperatly with "cert_create".
For example "TRUSTED_BOARD_BOOT=1" and "GENERATE_COT=0" at the time of build.
How to set "TRUSTED_BOARD_BOOT=1" without "TF_A_SIGN_ENABLE=1"?
Thank you.
Solved! Go to Solution.
2023-03-16 10:32 AM
Hi GChin.1 (Community Member)
Sorry for the late reply.
If you are only interested to test the secure boot, you don't need TRUSTED_BOARD_BOOT=1. You just want to sign your TF-A (TF_A_SIGN_ENABLE=1), in that case there is no need to sign the FIP.
Only If you've secure closed your chip (in OTP) , then you must build your TF-A with TRUSTED_BOARD_BOOT=1, it means that at build time TF-A will check that X509 certificates are present in the FIP. In Yocto it may means that having TF_A_SIGN_ENABLE=1 might also be linked to the FIP signature.
https://wiki.st.com/stm32mpu/wiki/How_to_perform_Secure_Boot_from_Distribution_package
You can refer to this page to sign your binaries before building the image, it is based on the OSTL DV4.1 but worth a try on DV3.1.1.
Regards,
Olivier
2023-03-16 10:32 AM
Hi GChin.1 (Community Member)
Sorry for the late reply.
If you are only interested to test the secure boot, you don't need TRUSTED_BOARD_BOOT=1. You just want to sign your TF-A (TF_A_SIGN_ENABLE=1), in that case there is no need to sign the FIP.
Only If you've secure closed your chip (in OTP) , then you must build your TF-A with TRUSTED_BOARD_BOOT=1, it means that at build time TF-A will check that X509 certificates are present in the FIP. In Yocto it may means that having TF_A_SIGN_ENABLE=1 might also be linked to the FIP signature.
https://wiki.st.com/stm32mpu/wiki/How_to_perform_Secure_Boot_from_Distribution_package
You can refer to this page to sign your binaries before building the image, it is based on the OSTL DV4.1 but worth a try on DV3.1.1.
Regards,
Olivier