cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I am trying to execute a simple ADC program(12bit) in stm32mp157c using trimpot with 10K as input in cube ide. Where output changes only at the voltage level of 3.2v

ASuha.1
Associate

While changing the value at the trimpot output values is constant(4095) and has no change as soon as when it reaches 3.2V it goes to zero. I am seeing output using uart.

Please assist me how to rectify it.​

1 REPLY 1
PatrickF
ST Employee

Hi,

May I suggest you to see if this post will help you : https://community.st.com/s/question/0D53W00000Y4kuGSAR/stm32mp157dk2-how-to-enable-vdda-and-vref-regulators

Regards.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.