cancel
Showing results for 
Search instead for 
Did you mean: 

EMMC device 0 not found

asadullah4571
Associate III

i try to flash starter package to our mmc but the error is found i done step by step

in botton text i bold the error please check it once and help me out why this is happend. 

 

 

 

 

10:55:11 : UR connection mode is defined with the HWrst reset mode
10:55:11 : USB speed : High Speed (480MBit/s)
10:55:11 : Manuf. ID : STMicroelectronics
10:55:11 : Product ID : DFU in HS Mode @Device ID /0x500, @Revision ID /0x0000
10:55:11 : SN : 004200273132511831373339
10:55:11 : DFU protocol: 1.1
10:55:11 : Board : --
10:55:11 : Device ID : 0x0500
10:55:11 : Start Embedded Flashing service
10:55:11 : Memory Programming ...
10:55:11 : Opening and parsing file: tf-a-stm32mp157f-dk2-usb.stm32
10:55:11 : File : tf-a-stm32mp157f-dk2-usb.stm32
10:55:11 : Size : 220.41 KB
10:55:11 : Partition ID : 0x01
10:55:11 : Download in Progress:
10:55:13 : File download complete
10:55:13 : Time elapsed during download operation: 00:00:01.818
10:55:13 : RUNNING Program ...
10:55:13 : PartID: :0x01
10:55:13 : Start operation done successfully at partition 0x01
10:55:13 : Memory Programming ...
10:55:13 : Opening and parsing file: fip-stm32mp157f-dk2-optee-sdcard.bin
10:55:13 : File : fip-stm32mp157f-dk2-optee-sdcard.bin
10:55:13 : Size : 1.40 MB
10:55:13 : Partition ID : 0x03
10:55:13 : Download in Progress:
10:55:15 : File download complete
10:55:15 : Time elapsed during download operation: 00:00:01.548
10:55:15 : RUNNING Program ...
10:55:15 : PartID: :0x03
10:55:15 : Reconnecting the device ...
10:55:19 : USB speed : High Speed (480MBit/s)
10:55:19 : Manuf. ID : STMicroelectronics
10:55:19 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
10:55:19 : SN : 004200273132511831373339
10:55:19 : DFU protocol: 1.1
10:55:19 : Board : --
10:55:19 : Device ID : 0x0500
10:55:19 : Device name : STM32MP157FAC Rev.Z
10:55:19 : Device type :
10:55:19 : Device CPU :
10:55:19 : Start operation done successfully at partition 0x03
10:55:19 : Flashlayout Programming ...
10:55:19 : Running Flashlayout Partition ...
10:55:19 : Reconnecting the device ...
10:55:19 : USB speed : High Speed (480MBit/s)
10:55:19 : Manuf. ID : STMicroelectronics
10:55:19 : Product ID : USB download gadget@Device ID /0x500, @Revision ID /0x2001, @Name /STM32MP157FAC Rev.Z,
10:55:19 : SN : 004200273132511831373339
10:55:19 : DFU protocol: 1.1
10:55:19 : Board : --
10:55:19 : Device ID : 0x0500
10:55:19 : Device name : STM32MP157FAC Rev.Z
10:55:19 : Device type :
10:55:19 : Device CPU :
10:55:19 : Flashlayout partition started successfully
10:55:19 : Error: Message from Embedded Flash Loader : mmc device 0 not found
10:55:19 : Received PhaseID == 0xFF, system is going to reboot
10:55:19 : Start Embedded Flashing service
10:55:19 : Error: Message from Embedded Flash Loader : mmc device 0 not found
10:55:19 : Received PhaseID == 0xFF, system is going to reboot

1 ACCEPTED SOLUTION

Accepted Solutions
Gregory PLANCHON
ST Employee

hi @asadullah4571,

 

There is no eMMC on boards stm32mp157f-dk2.

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Gregory PLANCHON
ST Employee

hi @asadullah4571,

 

There is no eMMC on boards stm32mp157f-dk2.

 

Regards,

Grégory

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.