2022-02-14 12:21 AM
Hi,
I create a QT project and run it on the board STM32MP157C-DK2 with command " /tmp/testqt/bin/testqt". The data display on the DSI display is mismatch my testing project's UI.
LCD_picture.jpg is DSI display data.
QT_UI.jpg is Qt project's UI.
Please advise how to solve it.
Thanks,
QiZhang
Solved! Go to Solution.
2022-02-15 7:00 AM
Hello @zqizh.1
Finally, your problem comes from a configuration of QtCreator itself. You need to configure the resolution of the target of the Designer tool.
How to do that ?
In QtCreator, go to Tools -> Options -> Designer -> Embedded Design.
Here you will create a new Device profile that will deals with your real target resolution. In the case of the native screen of the STM32MP15, we have something like 234 x 236 dpi.
Then you will restart QtCreator (it seems that it needs it to reconfigure the preview). And now the preview is in phase with what you can observe on your target:
Now you can adjust the font size of the QButton and the QLabel properly depending of what you want.
Hope it will help you.
Regards.
Erwan.
2022-02-14 12:30 AM
My LCD resolution is 480X800, and I configured the UI's geometry parameter to [(0,0),480x800]
2022-02-14 1:01 AM
2022-02-14 8:30 AM
Hello @zqizh.1 ,
I don't know why the geometry property doesn't work.
If you check the resolution of the screen by using modetest as explained in this page: https://wiki.st.com/stm32mpu/wiki/DRM_KMS_overview#Show_display_overall_status
By using the command
modetest -M stm
You can double check the resolution, but the only supported is 480x800, so it must be ok.
I don't have Qt installed so I can't test your project, but you can maybe try to force the geometry of your mainwindow to the size of the screen by calling in your constructor this:
resize(QDesktopWidget().availableGeometry(this).size());
Or you can check the current size of your mainwindow by displaying the value of the property "geometry" to check what is going on.
Regards,
Kevin
2022-02-15 2:45 AM
Hello @zqizh.1 and @Kevin HUBER,
I had QtCreator installed and linked with the ST Qt SDK. I can so reproduce the setup and I can observe the same things as @zqizh.1.
The resize option seems to be bypassed by the application, I think that EGLFS platform forces a sort of "fullscreen". We can observe it because if you configure the geometry with [0,0,200,300], you obtain exactly the same display on the screen.
@zqizh.1 can you share the different Qt environment variable that are configured on your board ? (enter the following command:
Board $> env | grep QT
)
Regards,
Erwan.
2022-02-15 7:00 AM
Hello @zqizh.1
Finally, your problem comes from a configuration of QtCreator itself. You need to configure the resolution of the target of the Designer tool.
How to do that ?
In QtCreator, go to Tools -> Options -> Designer -> Embedded Design.
Here you will create a new Device profile that will deals with your real target resolution. In the case of the native screen of the STM32MP15, we have something like 234 x 236 dpi.
Then you will restart QtCreator (it seems that it needs it to reconfigure the preview). And now the preview is in phase with what you can observe on your target:
Now you can adjust the font size of the QButton and the QLabel properly depending of what you want.
Hope it will help you.
Regards.
Erwan.
2022-02-15 11:58 PM
Hi Erwan,
Thank you very much.