2024-05-02 06:34 AM
Hi,
In a centralized network, the coordinator is the only entity able to permit network joining. If the coordinator power cycles, and starts up from persistence, does it maintain its coordinator status?
In my testing setup, when I power cycle the coordinator, it rejoins the network with the correct previous address. However, after requesting the network to permit joining (PermitJoinReq), new devices are not added to the network, when before power cycling it, they would. Does this means that it loses its status as a coordinator? My current guess is that it does and since it belongs to a centralized network, there isn't any other device with the authority to permit joining. However, the PermitJoinReq returns a success status.
What do you think could be happening?
I don't know what is going on, since I can't be sure of what actually happens when I call the persistent startup function from the ZSDK
2024-05-03 01:58 AM
Hi @Jorge Alves,
In a ZigBee centralized network both coordinator and routers can allow new devices to join the network when the permit join is enabled.
After restarting from persistence, the device is supposed to restore its configuration and takes back its role on the network.
Can you confirm that the association permit flag on the beacon response is set to true when a new device is attempting to join the network ? Could you please share a Wireshark capture ?
Which Wireless binary version you are using ?
Best regards,
Ouadi
2024-05-13 11:36 AM - edited 2024-05-13 11:36 AM
Hi @Ouadi ,
Sorry for the late response, I was and still am waiting on a sniffer. I will get back to you when it arrives.
2024-06-06 04:12 AM - edited 2024-06-11 05:41 PM
So, I finally got around to check this and for some reason the startup from persistence sequence is successful, but it seems to break some functionality. In the St wiki it explicitly says it restores the binding table and report configurations. In my application devices restored from persistence don't, and remaking a new bind request with the same entry doesn't work i just lose the reports and cant configure new ones hardcoded on device. Otherwise, the device works as expected with beacons, route requests, link status etc, but never reports again. The same was happening for performing a permit joining request from to the coordinator restored from persistence - returns as successful, but doesn't do anything.
It's on version 1.19.1 FFD for zigbee
2024-06-10 03:04 AM
Hi @Jorge Alves,
I can confirm that both reporting config and binding tables are saved into the NVM when the persistence mode is enabled, the reportable attribute should be configured with the flag ZCL_ATTR_FLAG_PERSISTABLE to be persisted.
Please follow the recommendation described on this AN Persistent data management ZigBee to implement properly this feature.
Regards,
Ouadi
2024-06-11 05:34 PM - edited 2024-06-11 05:40 PM
Again, thank you for the answer.
I am aware of the attribute flag, but I don't mind losing the attribute's value, I want to keep the report and binding information, or is it bound by that flag as well? It would be okay to not restore it as long as I would be able to keep or configure reportings again, which I am unable to do, while your API keeps returning Successful status at every request.
I am aware of the feature recommendations. I understand the features and followed your OnOff_NVM example for context. I am able to restore a device to a network by restarting it through the ZbStartupPersist function, and the device seems to restore its role on the network. However, I had problems in restoring the reporting configuration where before restarting would work and after they don't, while the network is kept the same otherwise. Even rebinding client and server and setting the report configurations again will not make the device ever report again.
I don't know how to proceed to solve the issue. If you cared to review, I could take some time to assemble a brief overview of the code to give you a better idea of the developed project, or even share the project, if you prefer. I might be overviewing or misunderstanding some simple detail.