Zigbee custom cluster fragmentation not working and sleep mode no wakeup
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-08 12:33 AM
Hey,
I have two problems regarding custom clusters and sleepy end devices. I want to create an SED that periodically sends custom long string messages (via attribute reporting) to a coordinator.
1.Question:
For this I implemented a custom cluster with a custom long string character attribute. For testing I only write to the attribute once the SED starts up.
enum ZclStatusCodeT status;
uint8_t Custom_str[255] = " PAYLOAD";
Custom_str[0] = 68; // length of string (ZCL format) LSB
Custom_str[1] = 0; // length of string (ZCL format) MSB
status = ZbZclAttrStringWriteLong(zigbee_app_info.custom_ls_server, MY_ZCL_DEV_LS, Custom_str);
APP_DBG("Attribute write status = %d", status);
This works as intended. My motivation to use the custom cluster was the ability to send long custom strings. If I change Custom_str[0] = 68; to Custom_str[0] = 100; the reporting stops and the message does not comes through (attributeWrite still successful). Fragmentation should be enabled by default in custom cluster, but apparently messages do not arrive in this configuration. Any hints on what might cause this issue are appreciated.
2.Question:
For the sleepiness of the end devices i oriented on the Zigbee_OnOff_Client_SED example. I enabled sleepy mode in the Zigbee Stack and made sure the following lines are present.
/* Enabling Stop mode */
UTIL_LPM_SetStopMode(1U << CFG_LPM_APP, UTIL_LPM_ENABLE);
UTIL_LPM_SetOffMode(1U << CFG_LPM_APP, UTIL_LPM_DISABLE);
Furthermore, NVIC configuration is the same. Despite this, the end devices do not wake up for performing the periodic long string attribute report. What might be the issue here?
Best regards and thanks for the help!
- Labels:
-
STM32WB series
-
Zigbee
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-08-06 9:26 AM
Hello @user5
Could you please provide more details and if possible, the logs of your errors. This may help our users.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-12-30 7:38 AM
Hi STTwo-32,
regarding the first question: i tried setting
ZbZclClusterSetTxOptions(zigbee_app_info.custom_ls_server, ZB_APSDE_DATAREQ_TXOPTIONS_SECURITY | ZB_APSDE_DATAREQ_TXOPTIONS_FRAG);
but this does not work too. Its hard to provide more information as the device is sleepy and thus does not return any logs. I am working with a STM32WB5MMG and for this device, there does not exist an example project. Maybe the error is reproducable with a string longer than 68 chars on the Zigbee_custom_ls_Server_Coord example project.
I was able to solve the second the second problem.
Thanks and best regards