2019-10-26 08:12 AM
while( 1 )
{
if (AppProcessRequest==LORA_SET)
{
/*reset notification flag*/
AppProcessRequest=LORA_RESET;
/*Send*/
Send( NULL );
}
if (LoraMacProcessRequest==LORA_SET)
{
/*reset notification flag*/
LoraMacProcessRequest=LORA_RESET;
LoRaMacProcess( );
}
/*If a flag is set at this point, mcu must not enter low power and must loop*/
DISABLE_IRQ( );
/* if an interrupt has occurred after DISABLE_IRQ, it is kept pending
* and cortex will not enter low power anyway */
if ((LoraMacProcessRequest!=LORA_SET) && (AppProcessRequest!=LORA_SET))
{
#ifndef LOW_POWER_DISABLE
LPM_EnterLowPower( );
#endif
}
ENABLE_IRQ();
}
Hi, I don't understand why I need to disable the IRQ before enter stop mode and enable it when the board wakes up, if I comment those functions (DISABLE_IRQ and ENABLE_IRQ) the node does not send or receive data properly
Thanks