Which MCUs supports for LoRa FUOTA ?
Hi fellas,
We are planning for LoRa based FUOTA updates using STM32 MCUs. The LoRa Transceiver we are planning to use is SX1302. In I-CUBE-LRWAN blog, they told its meant for STM32L0/1/4 series alone. Can we use some other series like STM32G0 series, for cost reasons? If not, what is the actual reason for it? As STM32G0 also has SPI interface, which can be interfaced to our Transceiver.
Also, as another hiccup, SX1302 has only HAL support, which works in Linux based Processor and no implementation idea has been given in terms of Controller? Any suggestions regarding that?