cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the list of Req_opcodes for Gatt_Error event

DS.4
Senior II

Hello

 

I am getting: error on opcode 0x08 what is it?

Opcodes not listed in document.

 

See here:

Table 433. ACI_GATT_ERROR_RESP_EVENT parameters
Parameter Size Description Possible values
Connection_Handle 2
Specifies the ATT bearer to
whom the command applies
• 0x0000 ... 0x0EFF: unenhanced ATT bearer (the parameter
is the connection handle)
• 0xEA00 ... 0xEA3F: enhanced ATT bearer (the parameter
LSB is the connection-oriented channel index)
Req_Opcode 1
The request that generated
the error response -

1 REPLY 1
STTwo-32
ST Employee

Hello @DS.4 

from what I understood of your explanation, I think you are looking for more details about the ACI_GATT_ERROR_RESP_EVENT event. I suggest you to take a look at the part 3.4.16 of the AN5270:

Screenshot_2023-11-14-21-22-25-34_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

If that doesn't answer your question, i suggest you give more details about your request.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.