2024-12-20 03:54 AM
Hello,
I would like to use the BLE_p2pServer_ota example with the STM32WBA55CG as a template for a project. Since I do not have an LSE available here, I would like to use the LSI. Which settings (defines) do I have to change?
If I use the LSI with 32,000kHz, the advertising works, but I cannot establish a connection.
2024-12-20 04:06 AM
Watch for LSI not running through power down, many STM32 only have LSE in the low power domain. Not sure if case here, but check RM